The Capacitive Sense Library (CSLIB) for EFM32 STK is described on table below.

For Gecko SDK Suite v2.0.0 (MCU 5.3.3.0), the cslib examples for different EFM32 STK are available here (Windows):

C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v2.0\app\mcu_example\KIT_NAME\cslib

where KIT_NAME is the name of the first column of above table.

More information for CSLIB can be found in AN0828 and AN0829 in Simplicity Studio or on www.silabs.com/32bit-appnotes.

  • Knowledge Base Articles
  • 32-bit MCUs