Member | Action | Date |
---|---|---|
|
Replied
to
ZWave700 Wireless Starter Kit : SimplicityStudio DebugAdapter not working
The following KB article originally written for EFM32 also applies for EFR32 devices. |
4 days ago |
|
Updated
to
Zwave 700 How can I use development board to program device
Vtarget is not a power supply, it is an input, and needed for level shifter reference and Vtarget measurement.
Show more
|
4 days ago |
|
Voted up hi_do_you_want_tousedevelopmentboardto-Exy1 Show more |
4 days ago |
|
Replied
to
Zwave 700 How can I use development board to program device
Vtarget is not a power supply, it is needed for level shifter reference and Vtarget measurement.
Show more
|
4 days ago |
|
Replied
to
The souce code of PC Controller can't be compiled
Yeah, looks like not all the source files are included in the latest Z-Wave PC Controller package. However, the source is not intended for customer's development, the gateway/controller reference design we offer is based on embedded Linux platforms, and as I known, we currently do not provide support for the DLL on Windows.
Show more
|
7 days ago |
|
Replied
to
SDK version 7.12.1 cannot be used for certification!
BTW, it is recommended using the latest SDK release for new products. User can use the "Other - Too new to be listed on form" field for new SDK version not listed on the certification form. |
9 days ago |
|
Voted up dont_know_the_reasonwhyitsayssobutisuspect-Pp1W Show more |
9 days ago |
|
Updated
to
Compliance testing tool , Device Emulator for Certification testing
I am able to get the Home ID after initializating the node without any other controller connecting. If using ZDP03A Z-Wave Development Platform, after programming the serialAPI Slave image into the Z-Wave device, make sure J3 and J4 are installed properly so that the UART interface of the Z-Wave device is connected to PC Host via USB1 port, that is, the J3 and J4 are set with 1 jumper each to pin2-pin3. |
15 days ago |
|
Updated
to
Compliance testing tool , Device Emulator for Certification testing
I am able to get the Home ID after initializating the node without any other controller connecting. If using ZDP03A Z-Wave Development Platform, after programming the serialAPI Slave image into the Z-Wave device, make sure J3 and J4 are installed properly so that the UART interface of the Z-Wave device are connected to PC Host via USB1 port, that is, the J3 and J4 are set with 1 jumper each to pin2-pin3. |
15 days ago |
|
Replied
to
Compliance testing tool , Device Emulator for Certification testing
I am able to get the Home ID after initialization the node without any other controller connecting. If using ZDP03A Z-Wave Development Platform, after programming the serialAPI Slave image into the Z-Wave device, make sure J3 and J4 are installed properly so that the UART interface of the Z-Wave device are connected to PC Host via USB1 port, that is, the J3 and J4 are set with 1 jumper each to pin2-pin3. |
15 days ago |