Member | Action | Date |
---|---|---|
|
Posted
Simplicity Studio 5 Parser Generates Syntax Error for `_Static_assert` on
Simplicity Studio Forum
I'm using `_Static_assert` for compile-time validation. When I build the project it builds with zero errors and zero warnings. However, the syntax parser in the editor flags my `_Static_assert` as having a syntax error. I already have the language mapping for C source files set to GNU C, as detailed in this post. How can I clear the syntax error warning?
|
16 days ago |
|
Voted up hi_vankata_that_isastrangeissueweseewitht-2MAd Show more |
30 days ago |
|
Posted
ERF32MG22 UART Bootloader on
32-bit MCU - Microcontroller Forum
Where can I find documentation of how to interface/use the example UART bootloader with the ERF32MG22? I have the Wireless Gecko dev kit and the bootloader-uart-bgapi example loaded. Where is the protocol used by the UART bootloader defined or--better yet--documented or--better yet--implemented as an example PC application? The closest that I have been able to find is this knowledge base article for the BLE drop-in modules. Is the protocol it outlines applicable to the bootloader-uart-bgapi example for ERF32MG22? Presumably not, so where is the protocol documented? |
Feb 19 2021, 11:49 PM |
|
Replied
to
Uninstall / Reinstall Simplicity Studio v5 on linux
@jpitt To get Simplicity Studio to appear in the Programming group on my system (Ubuntu 20.04) I had to set the Categories entry in studio.desktop to `Categories=GTK;Development;`. I noticed that Meld used this (working) assignment by default when I installed it.
Show more
|
Feb 09 2021, 9:39 PM |
|
Replied
to
Modify SS5 Thermometer Demo App to be Loaded OTA
@tenager Thanks for the response. Specifically, I am attempting to use the example projects Bluetooth - SoC Thermometer and SPI Flash Storage Bootloader (single image).
|
Feb 08 2021, 5:19 PM |
|
Replied
to
Are there any plans to update eclipse to a newer version?
@jpitt Which version/update of SS5 is supposed to support Eclipse Marketplace? I'm running v5.1.1, and I don't see the Eclipse Marketplace. |
Feb 05 2021, 8:35 PM |
|
Replied
to
Cannot successfully update adapter firmware
I am having the same problem updating firmware for my Gecko EFR32xG22 mainboard with Simplicity Studio 5 running on Ubuntu 20.04 (x64). I've tried the different methods described in this thread, but I still get the "Timed out waiting for kit to reset" error message. My log file is attached.
Show more
|
Jan 26 2021, 11:24 PM |