I want to connect to WSTK via Ethernet. WSTK is in a different subnet, ping is performed well
C:\Users\kuznecovav.ZAV>ping 192.168.2.16
Обмен пакетами с 192.168.2.16 по с 32 байтами данных:
Ответ от 192.168.2.16: число байт=32 время=1мс TTL=62
Ответ от 192.168.2.16: число байт=32 время<1мс TTL=62
Ответ от 192.168.2.16: число байт=32 время=2мс TTL=62
Ответ от 192.168.2.16: число байт=32 время<1мс TTL=62
Статистика Ping для 192.168.2.16:
Пакетов: отправлено = 4, получено = 4, потеряно = 0
(0% потерь)
Приблизительное время приема-передачи в мс:
Минимальное = 0мсек, Максимальное = 2 мсек, Среднее = 0 мсек
I made the settings in Simplicity Studio as shown below:
But in the "Debug Adapters" tab, my WSTK doesn't appear. Why it's happening? Can you help me, please?
If my WSTK is in the same subnet, then Simplicity Studio sees it
Discussion Forums
Simplicity Studio
Unanswered
Hi Alexandr,
You seem to be showing the settings and ping results for the working case on your subnet, but not for the non-working case, can you also show those settings?
Also on the [Device Manager] preferences please enable [Segger J-Link Ethernet UDP Discovery] and see if that helps:
That allows me to see WSTKs on different subnets on the VPN.
I put the laptop in the subnet where the WSTK is located. Therefore, the WSTK IP address remains unchanged.
I change the subnet configuration from '192.168.2.16' to '192.168.2.* and nothing changed.
0
Hi Alexandr,
The developer had a few suggestions.
1. Use either "Use TCP discovery for individual addresses" with 192.168.2.16 in the subnet configuration window OR "Include all network interfaces. (Use when connected to VPN)", but not both at the same time.
2. Can you telnet to port 4905 on ip address 192.168.2.16? That is the admin port for the WSTK and if you can telnet to it, then Simplicity Studio should detect the WSTK.
1. I began to use it separately "Use TCP discovery for individual addresses" и "Include all network interfaces. (Use when connected to VPN)".
2. My WSTK IP address has changed to 192.168.3.28
After entering the following command:
Microsoft Telnet> open 192.168.3.28 4905
I get the following:
Do I understand correctly that the connection is completed?
0
Hi Alexandr,
That screenshot seems to indicate a baud rate or other type of character encoding error. Instead of a screenshot, can you copy and paste from the terminal window to your reply?
I do not know if the Microsoft Telnet command 'term x' would help with the character encoding or not. The 'x' can be ansi, vt100, vt52 or vtnt. Type 'set ?' to see the usage.
I normal use the program 'Putty' for telnet and SSH connections. I do not know if that would work better for you or not.
In the previous message, I inserted the result after entering the command " set term vtnt"
With other types, too, nothing happened.
I get the same result on a computer that is located in the subnet 192.168.3.
Nothing has changed with Putty either.
0
In the penultimate message with the text from the terminal, I noticed that some of the labels match what I output to the log. This is for example "MIR S05-9469". Maybe it will be useful to you
0
Hi Alexandr,
The character encoding obviously looks wrong. These links might help in trying to change that:
Connect to WSTK over Ethernet
I want to connect to WSTK via Ethernet. WSTK is in a different subnet, ping is performed well
I made the settings in Simplicity Studio as shown below:
But in the "Debug Adapters" tab, my WSTK doesn't appear. Why it's happening? Can you help me, please?
If my WSTK is in the same subnet, then Simplicity Studio sees it
Hi Alexandr,
You seem to be showing the settings and ping results for the working case on your subnet, but not for the non-working case, can you also show those settings?
Also on the [Device Manager] preferences please enable [Segger J-Link Ethernet UDP Discovery] and see if that helps:
That allows me to see WSTKs on different subnets on the VPN.
Thank you,
jpitt
Hello jpitt,
Thanks for answer.
The first two images in the previous message are for a non-working case.
I enabled "Segger J-Link Ethernet UDP Discovery" but nothing changed.
Hi Alexandr,
Okay, I am a bit confused about the network topology since both the working and non-working case seem to use the same ip address: 192.168.2.16
If you are changing the subnet the WSTK is connected to, how do you keep that same ip address?
In the preferences if you change the subnet configuration from '192.168.2.16' to '192.168.2.*' does it help?
Thank you,
jpitt
Hello jpitt,
I put the laptop in the subnet where the WSTK is located. Therefore, the WSTK IP address remains unchanged.
I change the subnet configuration from '192.168.2.16' to '192.168.2.* and nothing changed.
Hi Alexandr,
The developer had a few suggestions.
1. Use either "Use TCP discovery for individual addresses" with 192.168.2.16 in the subnet configuration window OR "Include all network interfaces. (Use when connected to VPN)", but not both at the same time.
2. Can you telnet to port 4905 on ip address 192.168.2.16? That is the admin port for the WSTK and if you can telnet to it, then Simplicity Studio should detect the WSTK.
Thank you,
jpitt
Hello jpitt,
Sorry for delay.
1. I began to use it separately "Use TCP discovery for individual addresses" и "Include all network interfaces. (Use when connected to VPN)".
2. My WSTK IP address has changed to 192.168.3.28
After entering the following command:
I get the following:
Do I understand correctly that the connection is completed?
Hi Alexandr,
That screenshot seems to indicate a baud rate or other type of character encoding error. Instead of a screenshot, can you copy and paste from the terminal window to your reply?
I do not know if the Microsoft Telnet command 'term x' would help with the character encoding or not. The 'x' can be ansi, vt100, vt52 or vtnt. Type 'set ?' to see the usage.
I normal use the program 'Putty' for telnet and SSH connections. I do not know if that would work better for you or not.
Thank you,
jpitt
\(¤oъМ╤!][6 ┬Ъ)~№
ОхЎ¤фx▄ф!][ D├Ъ*У° ТWз∙є)ruoi][ъB├Ъ)Т№!вш¤з█'&!][Цю┬Ъ*П°Єдш∙∙з█'&i][Е├Ъ)Р№М№)Д№#ИХj¤\Ё.Щ!][oГ┬Ъ*Е° ▌┐У∙°\Ё.Щi][ХН┬Ъ)Ж№
░ #╞Z╘∙ўфx▄фi][R├Ъ)Ф№4°L¤сГР#!][╡S├Ъ*Х°ч■L∙їсГР#i][╜\├Ъ)Ц№
|∙ЁЬdЭUi][зР├Ъ)Ш№)#¤oъМ╤!][▌С├Ъ*Щ°·%∙№oъМ╤i][aз├Ъ)Ъ№╬~┼¤╠сkl!][Чи├Ъ*Ы°x┼∙сkli][Dй├Ъ+Ь╠сkl!][T┬├Ъ)Э№╝йа¤5╓╞3!][К├├Ъ*Ю°#-Qh∙√5╓╞3i][─Ъ)Я№{▓У¤\Ё.Щ!][ї ─Ъ*а°#х∙ы\Ё.Щi][;─Ъ)б№╟]│¤З╢Н!][q─Ъ*в°[│∙З╢Нi][─Ъ+гЗ╢Н!][√(─Ъ)д№▀M╨¤kL┴#!][2*─Ъ*е°
16¤-оФ!][--─Ъ*з° ╨76∙°-оФi][W─Ъ)и№""I¤Ц2╛ K╨∙ёkL┴#i][°+─Ъ)ж№
!][NX─Ъ*й°ё$I∙ёЦ2╛
\(¤oъМ╤!][Г┼Ъ*╡°° П.∙¤oъМ╤i][.┼Ъ)╢№#Лq┌¤╠сkl!][Щф─!][^/┼Ъ*╖°ihs┼∙√╠сkl№√юЎ¤фi][pH┼Ъ)╕№Ьhъ¤uвХфx▄фi][%┘─Ъ)░№
!][жI┼Ъ*╣°Onъ∙uвХ
ОхЎ¤фx▄ф"!][lQ╞Ъ*╩° ]уЎ∙°фx▄ф"i][╦_╞Ъ)╦№4°L¤сГР!][a╞Ъ*╠°ч■L∙∙сГРi][┼Ъ+╞з█'!][╤╞Ъ)╟№ i][eП┼Ъ)║№
░ j╞Ъ)═№
╔ва¤5╓╞3!][╓╨╞Ъ*╘°)#да∙∙5╓╞3i][╞Ъ*╨°·%∙°oъМ╤i][о┤╞Ъ)╤№╬~┼¤╠сkl!][ф╡╞Ъ*╥°#Е`∙·╠сkli][а╧╞Ъ)╙№
╟Ъ)╒№{▓У¤\Ё.Щ!][A╟Ъ*╓°и┤У∙°\Ё.Щi][И!╟Ъ)╫№╟]│¤З╢Н!][╛"╟Ъ*╪°#бyЩ∙√З╢Нi][G6╟Ъ)┘№▀M╨¤kL┴#!][Б7╟Ъ*┌°
16¤-оФ!][z:╟Ъ*▄° ╨76∙Ў-оФi][ed╟Ъ)▌№""I¤Ц2╛ !][Ыe╟Ъ*▐°ё$I∙ЎЦ2╛ i][SБ╟Ъ)▀№#▒┤w¤з█'!][йВ╟Ъ*р° Зпш∙¤з█'i][wЩ╟Ъ)с№4Zз¤)ruo!][нЪ╟Ъ*т°ч\з∙°)ruoi][ZЫ╟Ъ+у)ruo!][AMл╟Ъ*ф°B%ЄGNГ.> 6ь)№№ЫvFb║Y))J
ЫH╜T╤щcъ¤uвХ╚Ъ)я№°╨hs┼∙№╠сkl.∙№oъМ╤i][T;╚Ъ)э№┼|¤ЬdЭU!][цё╟Ъ*ъ°|∙ўЬdЭUi][Ъ$╚Ъ)ы№
!!][ЄV╚Ъ*Ё° :eъ∙uвХ
!i][ЯW╚Ъ+ёuвХ
кF╨¤kL┴#!][%╛╚Ъ*ў° y@╨∙єkL┴#i][ъ┐╚Ъ)°№v:6¤-оФ !][ ┴╚Ъ*∙°е<6∙∙-оФ i][╠┴╚Ъ+·-оФ !][
W)I¤Ц2╛!][-ь╚Ъ*№° Д/I∙ЎЦ2╛i][эь╚Ъ+¤Ц2╛!][∙╔Ъ)■№!вш¤з█' ы╚Ъ)√№
!][/ ╔Ъ*#╚▒╨∙∙з█'
░хЎ¤фx▄ф!][╕^╔Ъ*° ]уЎ∙юфx▄фi][m╔Ъ)№4°L¤сГР!][Nn╔Ъ*°ч■L∙ЇсГРi][Vw╔Ъ)№ i][ ╔Ъ)№#diI¤)ruo!][s!╔Ъ*° ТWз∙ё)ruoi][В]╔Ъ)№
|∙°ЬdЭUi][@л╔Ъ№)#¤oъМ╤!][vм╔Ъ* °·%∙ЇoъМ╤i][√┴╔Ъ)
№╬~┼¤╠сkl!][0├╔Ъ*
°x┼∙є╠сkli][э▄╔Ъ)
°oпа∙¤5╓╞3!i][X#╩Ъ)№{▓У¤\Ё.Щ !][О$╩Ъ*°и┤У∙Ў\Ё.Щ i][╘.╩Ъ)№╟]│¤З╢Н!][ №╝йа¤5╓╞3!!][#▐╔Ъ*
0╩Ъ*°[│∙ЄЗ╢Нi][УC╩Ъ)№▀M╨¤kL┴#!][╦D╩Ъ*°
K╨∙∙kL┴#i][РF╩Ъ)№#@Ча¤-оФ!][цG╩Ъ*° ╨76∙∙-оФi][▒q╩Ъ)№#ё┤?¤Ц2╛!][s╩Ъ*°ё$I∙ЎЦAєL¤сГР!!][ЇЇ╩Ъ*° ТїL∙°сГР!i][№¤╩Ъ) №┼|¤ЬdЭU!][·з╩Ъ*°#м▀Ё∙ў)ruoi][)ф╩Ъ)№√юЎ¤фx▄ф&!][_х╩Ъ*°(шЎ∙їфx▄ф&i][╛є╩Ъ)№
!][2Ъ*!°|∙яЬdЭU
╗u┼¤╠сkl!][╓I╦Ъ*&° hs┼∙■╠сkli][╦Ъ+$oъМ╤c╦Ъ)'№#┬╨d¤uвХ i][ц1╦Ъ)"№
!][_d╦Ъ*(°Onъ∙uвХ
W)I¤Ц2╛!][Н∙╦Ъ*0°,° aP│∙·З╢Нi][6═╦Ъ)-№v:6¤-оФ!][l╬╦Ъ*.°#dyq∙№-оФi][W°╦Ъ)/№i][■й╦Ъ))№
░хЎ¤фx▄ф!][l╠Ъ*6°4°wП]уЎ∙√фx▄фi][dz╠Ъ)7№4°L¤сГР!][Ъ{╠Ъ*8°ч■L∙∙сГРi][вД╠Ъ)9№
щcъ¤uвХi][ЕЖ╠Ъ+;ЬdЭU!][М╕╠Ъ)<№#эd]¤oъМ╤"!][▐╣╠Ъ*=°·%∙тoъМ╤"i][G╧╠Ъ)>№╬~┼¤╠сk!][}╨╠Ъ*?°x┼∙√╠сki][пщ╠Ъ)@№
!][хъ╠Ъ*A°
#№яf∙uвХ
Tйш¤з█'!]["Э═Ъ*M° Зпш∙Єз█'i][┤═Ъ)N№4Zз¤)ruo!!][F╡═Ъ*O°ч\з∙ш)ruo[i][uё═Ъ)P№√юЎ¤фx▄ф!][лЄ═Ъ*Q°(шЎ∙ффx▄фi][)F№
AєL¤сГР!][@╬Ъ*S° ТїL∙ЎсГРi][ь╬Ъ+TсГР!][H ╬Ъ)R№
╬Ъ)U№#Р%9¤ЬdЭ!][Ю
\(¤oъМ╤!][h@╬Ъ*X° ╬Ъ*V°|∙єЬdЭi][2?╬Ъ)W№
▓V│¤З╢Н!][№├╬Ъ*a°#aP│∙°З╢Нi][Ж╫╬Ъ)b№▀M╨¤kL┴#!][┐╪╬Ъ*c°
W)I¤Ц2╛!][┌╧Ъ*g° Д/I∙ЇЦ2╛i][Т"╧Ъ)h№!вш¤з█' K╨∙ёkL┴#i][Г┌╬Ъ)d№v:6¤-оФ"!][╣█╬Ъ*e°е<6∙ў-оФ"i][д╧Ъ)f№
!][╚#╧Ъ*i°Єдш∙∙з█'
░хЎ¤фx▄ф!][Qy╧Ъ*m° ]уЎ∙ўфx▄фi][■y╧Ъ+nфx▄ф!][▒З╧Ъ)o№#─о¤сГР#!][Й╧Ъ*p°ч■L∙їсГР#i][яС╧Ъ)q№
!][%У╧Ъ*r°
i][┘┼╧Ъ)s№)#¤oъМ╤ !][╟╧Ъ*t°·%∙яoъМ╤ i][У▄╧Ъ)u№╬~┼¤╠сkl!][╒┐▌╧Ъ*v°└x┼Є∙ш"0%я─gНbU▒}Йfїо0eQ╖√2(ъF╗&В▀═╟╤╘Oй$8Бьх2B&8Т┘!g°(+]L╛}▒·ЕUцKПfЬg{ъ▒MшPГ?┘NBЬмRJ&╚Y╝/`T6я╬LЬFPW
┬З
тUYDT╟╔т▄╙█ДJ▄а= 3i╔╕Jй:jВ7KЎ√eуtDЯ▀а∙ЗKНя╓┬C╛╝яОUpТ|╣(Уa└═s_R└·└орйOдчx*у┘·][`ф╧Ъ)w№╬~┼¤╠сkl!][№Ў╧Ъ)x№Ьhъ¤uвХ
!][2°╧Ъ*y°Onъ∙uвХ
i][Am·╧Ъ*z°B%мД Ў╡ dY│*Юь╜d`├ыьFшг╢#;╘Г└∙▐╓╛ЙО
i][ё=╨Ъ){№{▓У¤\Ё.Щ!][&?╨Ъ*|°и┤У∙ї\Ё.Щi][╥?╨Ъ+}\Ё.Щ!][mI╨Ъ)~№╟]│¤З╢!]
Tйш¤з█'!][nк╨Ъ*З°^╨Зпш∙Єз█'i][]┴╨Ъ)И№4Zз¤)ruo!][Т┬╨Ъ*Й°ч\з∙є)ruoi][┬■╨Ъ)К№#А
AєL¤сГР!][М╤Ъ*Н° ∙¤фx▄ф!][╤Ъ*Л°(шЎ∙Ўфx▄фi][W╤Ъ)М№
▓V│¤З╢Н!][H╤╤Ъ*Ъ°i]aP│∙З╢Нi][╥ф╤Ъ)Ы№▀M╨¤kL┴#!][)У№▌┐У∙э\Ё.Щi][╨╤Ъ)Щ№╤Ъ*Ф°oпа∙·5╓╞3$i][Aб╤Ъ*Х°B%мД Ў╡└ dY│*Юь╜d`├ыьFшг╢#;╘Г└·┌╓╛ЙОi][)▓з╤Ъ*Ц°
ц╤Ъ*Ь°
ОхЎ¤фx▄ф!][ЭЖ╥Ъ*ж° ТWз∙ў)ruoi][hЕ╥Ъ)е№!вш¤з█'!][1╥Ъ*в°Єдш∙∙з█'i][H╥Ъ)г№:6¤-оФ!][щ╤Ъ*Ю°е<6∙є-оФi][Ё╥Ъ)Я№
░ #╞Z╘∙ўфx▄фi][¤Ф╥Ъ)з№4°L¤сГР!][3Ц╥Ъ*и°ч■L∙ўсГРi][;Я╥Ъ)й№
╔ва¤5╓╞3%!][╙Ъ*▒°° hs┼∙¤╠сkl i][┬ы╥Ъ+п╠сkl !][╥╙Ъ)░№
MIR S05-1542Re{∙ч╓╛ЙОi][ш∙Єз█'i][й╬╙Ъ)┐№4Zз¤)ruo!][▀╧╙Ъ*└°ч\з∙Ї)ruoi][3]у╙Ъ*┴° °╔Хr\!][яW╙Ъ*╡°[│∙ьЗ╢Н i][ЫX╙Ъ+╢З╢Н !][xk╙Ъ)╖№
щcъ¤uвХ!][┘╘Ъ*┼°╘Ъ)ТїL∙їсГРi][т%╘Ъ)╞№┼|¤ЬdЭU"!]['╘Ъ*╟°|∙эЬdЭU"i][╦Y╘Ъ)╚№)#¤oъМ╤#!][√Z╘Ъ*╔°·%∙┌oъМ╤#i][Еp╘Ъ)╩№#╫J=¤╠сkl !][▄q╘Ъ*╦°x┼∙¤╠сkl i][юК╘Ъ)╠№
!][$М╘Ъ*═° :eъ∙uвХ
╣У¤\Ё.Щ!][╙╘Ъ*╧° ▌┐У∙°\Ё.Щi][`▌╘Ъ)╨№#Яw¤З╢Н!][╢▐╘Ъ*╤° aP│∙∙З╢Нi][Є╘Ъ)╥№▀M╨¤kL┴#!][Wє╘Ъ*╙°
░хЎ¤фx▄ф"!][ъУ╒Ъ*▐° ]уЎ∙°фx▄ф"i][Jв╒Ъ)▀№4°L¤сГР!][г╒Ъ*р°ч■L∙∙сГРi][Им╒Ъ)с№ K╨∙∙kL┴#i][ї╘Ъ)╘№v:6¤-оФ!][MЎ╘Ъ*╒°е<6∙я-оФi][< ╒Ъ)╓№
╗u┼¤╠сkl!][b°╒Ъ*ц° П.∙щoъМ╤%i][,ў╒Ъ)х№
#F
16¤-оФ!][°|╓Ъ*ё° ╨76∙Ў-оФi][тж╓Ъ)Є№""I¤Ц2╛!][и╓Ъ*є°ё$I∙ЁЦ2╛i][╤├╓Ъ)Ї№#╪╫н¤з█'!][)┼╓Ъ*ї°X╓Ъ)ъ№Зпш∙·з█'i][ї█╓Ъ)Ў№4Zз¤)ruo!][+▌╓Ъ*ў°ч\з∙ь)ruoi][╫▌╓Ъ+°)ruo!][[╫Ъ)∙№√юЎ¤фx▄ф
!][С╫Ъ*·°(шЎ∙Ўфx▄ф
i][
i][╥}╫Ъ)№╬~┼¤╠сkl!][╫Ъ*°x┼∙╠сkli][:Ш╫Ъ)№Ьhъ¤uвХd4╫Ъ*■°|∙ЎЬdЭU&i][g╫Ъ))#¤oъМ╤
#!][pЩ╫Ъ*°Onъ∙uвХ
#i][Ъ╫Ъ+uвХ
#!][A)▒╫Ъ*°B%ЄGNГ.> 6ь)№№ЫvFb║Y))J
▓V│¤З╢Н !][╧ы╫Ъ* ▌┐У∙ў\Ё.i][мъ╫Ъ) № ЫH╜T╤▓_цФ~∙▌╓╛ЙО'i][0▀╫Ъ)№
° aP│∙ыЗ╢Н i][kЪ)
№▀M╨¤kL┴#!][е╪Ъ*
°
ОхЎ¤фx▄ф!][6б╪Ъ*°Ъ*°е]уЎ∙ёфx▄фi][Цп╪Ъ)№4°L¤сГР!][╠░╪Ъ*°ч■L∙°сГРi][╘╣╪Ъ)№░╨∙Їз█'i][Ьb╪Ъ)№#╨8■¤)ruo!!][Єc╪Ъ*° ТWз∙°)ruo!i][а╪Ъ)№
|¤ЬdЭU!!][
╔ва¤5╓╞3!][а ┘Ъ*"° да∙Ё5╓╞3i][A=I┘Ъ*#°B%ЄGNГ.> 6ь)№№ЫvFb║Y))J ╗╪Ъ*° c
ЫH╜T╤▓_цФ|·╪╓╛ЙО
Tйш¤з█'!][S╥┘Ъ*/°Rq┘Зпш∙√з█'i][Bщ┘Ъ)0№4Zз¤)ruo#!][xъ┘Ъ*1°#м▀Ё∙∙)ruo#i][з&┌Ъ)2№√юЎ¤фx▄фЦ2╛!][Е╡┘Ъ*-°ё$I∙ЎЦ2╛i][╤┘Ъ).№
!][▌'┌Ъ*3°(шЎ∙ўфx▄ф
AєL¤сГР$!][r7┌Ъ*5° ТїL∙їсГР$i][z@┌Ъ)6№┼|¤ЬdЭU!][░A┌Ъ*7°|∙ЁЬdЭUi][dt┌Ъ)8№)#¤oъМ╤!][Ъu┌Ъ*9°·%∙ЄoъМ╤i][Gv┌Ъ+:oъМ╤!][Л┌Ъ);№╬~┼¤╠сkl!][TМ┌Ъ*<°x┼∙╠сkli][Зе┌Ъ)=№#ўИY¤uвХ
!][▌ж┌Ъ*>° :eъ∙uвХ
i][
!][√;█Ъ*F°#dyq∙Є-оФaP│∙З╢Нi][╡█Ъ)C№v:6¤-оФ
░хЎ¤фx▄ф!][Го█Ъ*L°!]уЎ∙ўфx▄фi][т╝█Ъ)M№4°L¤сГР!][╛█Ъ*N°ч■L∙ўсГРi][!╟█Ъ)O№
|∙ЁЬdЭUi][╔█Ъ+QЬdЭU!][
╗u┼¤╠сkl&!][·▄Ъ*U° hs┼∙■╠сkl&i][-,▄Ъ)V№Ьhъ¤uвХ№█Ъ*S° П.∙ЇoъМ╤i][┼▄Ъ)T№
!][c-▄Ъ*W°#?Г▐∙uвХ
i]["s▄Ъ)X№{▓У¤\Ё.Щ!][Xt▄Ъ*Y°и┤У∙°\Ё.Щi][Ю~▄Ъ)Z№╟]│¤З╢Н!][╘▄Ъ*[°[│∙√З╢Нi][^У▄Ъ)\№▀M╨¤kL┴##!][ХФ▄Ъ*]°
AєL¤сГР!][╛D▌Ъ*i° ТїL∙∙сГРi][kE▌Ъ+jсГР!][╟M▌Ъ)k№#▄\T¤ЬdЭU!][O▌Ъ*l°|∙°ЬdЭUi][▒Б▌Ъ)m№)#¤oъМ╤"!][█В▌Ъ*n°#Bh K╨∙·kL┴##i][[Ц▄Ъ)^№
∙▀oъМ╤"i][kШ▌Ъ)o№╬~┼¤╠сkl!][бЩ▌Ъ*p°x┼∙¤╠сkli][]│▌Ъ)q№╝йа¤5╓╞3!][У┤▌Ъ*r°oпа∙·5╓╞3
░хЎ¤фx▄ф!][╧╗▐Ъ*Г°∙▌]уЎ∙ыфx▄фi][{╝▐Ъ+Дфx▄ф!][/╩▐Ъ)Е№#╩Ъn¤сГР!][Е╦▐Ъ*Ж°ч■L∙°сГРi][m╘▐Ъ)З№
|¤ЬdЭU!][г╒▐Ъ*И°
щcъ¤uвХl!][G ▀Ъ*М°#hs┼∙сkli][y9▀Ъ)Н№][▀Ъ)Л№
i][ка▀Ъ)У№▀M╨¤kL┴#!][сб▀Ъ*Ф°дБ▀Ъ*П°и┤У∙є\Ё.Щ$i][PВ▀Ъ+Р\Ё.Щ$!][ыЛ▀Ъ)С№╟]│¤З╢Н
Tйш¤з█'!][ьь▀Ъ*Ъ° Зпш∙ўз█'i][█рЪ)Ы№4Zз¤)ruo!][·╧▀Ъ*Ш°ё$I∙ЁЦ2╛#i][╢ы▀Ъ)Щ№
!][рЪ*Ь°ч\з∙х)ruo
i][Ab"рЪ*Э°B%мД Ў╡ dY│*Юь╜d`├ыьFшг╢#;╘Г└∙▀╓╛ЙО
AєL¤сГР&!][ i][?AрЪ)Ю№#О8Ф¤фx▄ф!][ХBрЪ*Я°(шЎ∙юфx▄фi][╒PрЪ)а№
RрЪ*б°
щcъ¤uвХ #"з∙ЎсГР&i][[рЪ)в№┼|¤ЬdЭU!][I\рЪ*г°|∙∙ЬdЭUi][¤ОрЪ)д№)#¤oъМ╤!][3РрЪ*е°·%∙ЇoъМ╤i][╖ерЪ)ж№╬~┼¤╠сkl!][эжрЪ*з°x┼∙╠сkli][ └рЪ)и№
!][U┴рЪ*й° :eъ∙uвХ
AQз¤)ruo!][дVсЪ*│°° Д/I∙ЄЦ2╛i][]rсЪ)┤№!вш¤з█'!][УsсЪ*╡°Єдш∙¤з█'i][БКсЪ)╢№)▓№сЪ)м№
!][│ЛсЪ*╖° ТWз∙щ)ruo
ОхЎ¤фx▄ф!][╔сЪ*║°[ц╟сЪ)╣№ i][3╙гсЪ*╕° ф=Ю.Д
░ #╞Z╘∙юфx▄фi][{╫сЪ)╗№4°L¤сГР&!][▒╪сЪ*╝°ч■L∙їсГР&i][╣ссЪ)╜№
]Ї$╪УX_{ы∙р╓╛ЙОoъМhs┼∙╠сkli][@.тЪ+├╠сkl!][PGтЪ)─№#√Ў¤5╓╞3!][еHтЪ*┼° да∙∙5╓╞3i][)ПjтЪ*╞°
i][╗НтЪ)╟№{▓У¤\Ё.Щ!][ёОтЪ*╚°#х∙я\Ё.Щi][7ЩтЪ)╔№╟]│¤З╢Н!][mЪтЪ*╩°[│∙∙З╢Нi][ЫтЪ+╦З╢Н!][ЎнтЪ)╠№▀M╨¤kL┴#$!][.птЪ*═°
AQз¤)ruo%!][ЩфЪ*Ё° ТWз∙·)ruo%i][A▓вфЪ*ё°B%ЄGNГ.>[▀АфЪ 6ь)№№ЫvFb║Y))J[ЛБфЪ+юз█'%!][═ЧфЪ)я№Ъ*▌°·%∙√oъМ╤i][│уЪ)▐№#░К¤╠сkl%!][Y┤уЪ*▀°x┼∙■╠сkl%i][Ў═уЪ)р№╝йа¤5╓╞3!][,╧уЪ*с°#-Qh∙№5╓╞3i][aфЪ)т№
ЫH╜T╤▓_цФ~∙┌╓╛ЙО
░хЎ¤фx▄ф!][h╓фЪ*є° ]уЎ∙юфx▄фi][╟ффЪ)Ї№4°L¤сГР!][¤хфЪ*ї°ч■L∙ўсГРi][яфЪ)Ў№ i][2╒фЪ)Є№
╗u┼¤╠сkl!][р:хЪ*√°$хЪ*∙° П.∙°oъМ╤ i][к9хЪ)·№
#F
в∙№╠сkli][TхЪ)№№Ьhъ¤uвХ
!][HUхЪ*¤°Onъ∙uвХ
i][ЫхЪ)■№{▓У¤\Ё.Щ !][=ЬхЪ*и┤У∙ї\Ё.Щ i][ДжхЪ)№╟]│¤З╢Н$!][╣зхЪ*°#бyЩ∙ЄЗ╢Н$i][C╗хЪ)№▀M╨¤kL┴#!][}╝хЪ*°
16¤-оФ!][v┐хЪ*° ╨76∙√-оФi][aщхЪ)№""I¤Ц2╛ K╨∙їkL┴#i][@╛хЪ)№
!][ЧъхЪ*°ё$I∙ёЦ2╛
i][OцЪ№#х└¤з█'!][ецЪ* ° Зпш∙№з█'i][tцЪ)
№4Zз¤)ruo!][йцЪ*
°ч\з∙ё)ruoi][V цЪ+
W)I¤Ц2╛ !][=qчЪ*$°°У∙Д/I∙ЎЦ2╛ i][щqчЪ+%Ц2╛ !][їМчЪ)&№!вш¤з█'!][+ОчЪ*'°#╚▒╨∙·з█'i][ечЪ)(№#<·%∙ъoъМ╤!i][P└цЪ)№╬~┼¤╠сkl!][Ж┴цЪ*°x┼∙№╠сkli][C█цЪ)№ )ruo!][3O2цЪ*
ОхЎ¤фx▄ф!][┤учЪ*+° ]уЎ∙Ёфx▄фi][ЄчЪ),№4°L¤сГР
!][JєчЪ*-°ч■L∙°сГР
░ i][R№чЪ).№
щcъ¤uвХl!!][,HшЪ*3° hs┼∙¤╠сkl!i][_aшЪ)4№
!][ХbшЪ*5° :eъ∙uвХ
i][AcшЪ+6uвХ
!][TишЪ)7№{▓У¤\Ё.Щ#!][ЙйшЪ*8°и┤У∙є\Ё.Щ#i][╨│шЪ)9№╟]│¤З╢Н!][╡шЪ*:°[│∙ЄЗ╢Нi][П╚шЪ);№▀M╨¤kL┴#!][╟╔шЪ*<°
K╨∙ЇkL┴#i][М╦шЪ)=№#@Ча¤-оФ !][т╠шЪ*>° ╨76∙ў-оФ i]
W)I¤Ц2╛!][y~ъЪ*W°°][aP│∙√З╢Нi][2RъЪ)T№v:6¤-оФ!][hSъЪ*U°#dyq∙ў-оФi][S}ъЪ)V№√oъМ╤i][─╕щЪ+LoъМ╤!][Ь═щЪ)M№╬~┼¤╠сkl!][╥╬щЪ*N°x┼∙╠сkli][ПшщЪ)O№╝йа¤5╓╞3!][·.ъЪ)P№
ОхЎ¤фx▄ф!][ёъЪ*]°°#w]уЎ∙юфx▄фi][`Ъ)^№4°L¤сГР!][ЖыЪ*_°ч■L∙ЎсГРi][Юf▓ъЪ)ZыЪ)`№┼|¤ЬdЭU$!][╨
ыЪ*a°|∙ЄЬdЭU$i][Б
Tйш¤з█'$!]["ьЪ*t° Зпш∙√з█'$i][ьЪ)q№""I¤Ц2╛$!][/ьЪ*r°ё$I∙ЁЦ2╛$i][ш ьЪ)s№Ъ)i№{▓У¤\Ё.Щ!][╓╢ыЪ*j°и┤У∙щ\Ё.Щi][┴ыЪ)k№╟]│¤З╢Н#!][N┬ыЪ*l°[│∙ЄЗ╢Н#i][▄╒ыЪ)m№ П.∙°oъМ╤i][DTыЪ)e№
i][.─ьЪ)~№)#¤oъМ╤° ТїL∙∙сГРi][щЗьЪ+{сГР!][EРьЪ)|№#xOi¤ЬdЭUuo i][qvьЪ)w№√юЎ¤фx▄ф!][зwьЪ*x°(шЎ∙№фx▄фi][ЖьЪ)y№
!][d┼ьЪ*°#Bh
∙ўoъМ╤
i][щ┌ьЪ)А№╬~┼¤╠сkl!][▄ьЪ*Б°x┼∙■╠сkli][QїьЪ)В№#vБ╙¤uвХ
$!][зЎьЪ*Г°Onъ∙uвХ
▓V│¤З╢Н!][∙HэЪ*И° aP│∙З╢Нi][В\эЪ)Й№▀M╨¤kL┴#!][╣]эЪ*К° $i][A]эЪ*Д°B%мД Ў5 `[│*■ь╜d`Ф├ыюшг╢#СЭ[╘Г└·█╓╛ЙОi][G<эЪ)Е№
MIR S05-9469Ъ├∙Є╓╛ЙО ТWз∙ы)rui][3№╟эЪ*У° с╥Хr\][─иэЪ*Р°Єдш∙∙з█'i][▓┐эЪ)С№v:6¤-оФ !][а`эЪ*М°е<6∙ш-оФ i][аКэЪ)Н№
ОхЎ¤фx▄ф!][M■эЪ*Х°i]]уЎ∙∙фx▄фi][·■эЪ+Цфx▄ф!][н
\(¤oъМ╤!][з?∙ЄЬdЭU юЪ)Ч№#~╦┘¤сГР !][юЪ*Ш°ч■L∙ўсГР i][ыюЪ)Щ№┼|¤ЬdЭU
щcъ¤uвХl!][┼bюЪ*Ю° hs┼∙Ў╠сkli][ў{юЪ)Я№
%!][.}юЪ*а°
#№яf∙uвХ
%i][AэЩюЪ*б°B%мД Ў╡ dY│*Юь╜d`├ыьFшу╢#;╘Л─·╫╓╛ЙО'i][э┬юЪ)в№{▓У¤\Ё.Щ
!][#─юЪ*г°и┤У∙Ў\Ё.Щ
i][╧─юЪ+д\Ё.Щ
AєL¤сГР!][ЙФяЪ*╡°╛ГяЪ)▓№#4]N¤фx▄ф%!][ЕяЪ*│°(шЎ∙Ўфx▄ф%i][SУяЪ)┤№i][3YSяЪ*▒° dЖG'qД !][i╬юЪ)е№╟]│¤З╢Н!][Я╧юЪ*ж°[│∙З╢Нi][(уюЪ)з№
░ #"з∙∙сГРi][СЭяЪ)╢№
|¤ЬdЭU
|∙юЬdЭU!][├ЮяЪ*╖° c
╔ва¤5╓╞3!][^ЁЪ*╜°#¤да∙∙5╓╞3i][Ъ*╣°·%∙рoъМ╤"i][5шяЪ)║№╬~┼¤╠сkl!][kщяЪ*╗°x┼∙╠сkli][(ЁЪ)╝№
MIR S05-1542=п∙ё╓╛ЙО ЁЪ+╛5╓╞3!][3Z
▓V│¤З╢Н!][EVЁЪ*├°][aP│∙З╢Нi][╬iЁЪ)─№▀M╨¤kL┴#!!][kЁЪ*┼°Ї\Ё.Щi][UЁЪ)┬№
NPO"MIR"Х)b∙√╓╛ЙО'i][dТWз∙ї)ruoi][3WцЁЪ*╬° ф=Ю.Д[╢ЁЪ*╦°Єдш∙■з█'i][ЁЪ)╠№№v:6¤-оФ!][nЁЪ*╟°е<6∙№-оФi][ьЧЁЪ)╚№
╗u┼¤╠сkl!][pёЪ*╫°╒°4°hs┼∙╠сkli][╛pёЪ+╪╠сkl!][DЙёЪ)┘№Ьhъ¤uвХ¤ЬdЭU!][m%ёЪ*╙°|∙ЇЬdЭUi][!XёЪ)╘№
!][zКёЪ*┌°Onъ∙uвХ
Tйш¤з█'&!][╢<ЄЪ*ч° Зпш∙∙з█'&i][еSЄЪ)ш№4Zз¤)ruo!][╚ЄЪ*х°ё$I∙ЁЦ2╛i][Б;ЄЪ)ц№i][9╨ёЪ)█№{▓У¤\Ё.Щ!][o╤ёЪ*▄°#х∙Ё\Ё.Щi][╡█ёЪ)▌№╟]│¤З╢Н !][ы▄ёЪ*▐°[│∙ьЗ╢Н i][Ч▌ёЪ+▀З╢Н !][uЁёЪ)р№
ОхЎ¤фx▄ф&!][@ТЄЪ*ъ° СЄЪ)щ№
░єL¤сГР!][╒бЄЪ*ь°#ТїL∙∙сГРi][▐кЄЪ)э№
|∙ўЬdЭUi][╟▐ЄЪ)я№)#¤oъМ╤
!][¤▀ЄЪ*Ё°·%∙ўoъМ╤
╣У¤\Ё.Щ!][XєЪ*ў°О'i]▌┐У∙Ї\Ё.Щi][\bєЪ)°№#^-а¤З╢НЄЪ)ё№#╛)ч¤╠сkl!][╫ЎЄЪ*Є°x┼∙°╠сkli][tєЪ)є№#УЄ|¤5╓╞3 !][╩єЪ*Ї°oпа∙ї5╓╞3 i][)]1єЪ*ї°
!][▓cєЪ*∙° aP│∙З╢Н
W)I¤Ц2╛!][nжєЪ*■° Д/I∙ўЦ2╛i]['┬єЪ)!вш¤з█'!][]├єЪ*°Єдш∙·з█'i][ i][єЪ)·№▀M╨¤kL┴#!][zєЪ)√№v:6¤-оФ!][F{єЪ*№°е<6∙∙-оФi][9еєЪ)¤№
─єЪ+з█'!][K┌єЪ)№4Zз¤)ru!][o█єЪ*°ч\з∙ы)rui][░ЇЪ)№√юЎ¤фx▄ф
!][цЇЪ*°(шЎ∙ўфx▄ф
i][F'ЇЪ)№4°L¤сГР$!][{(ЇЪ*°ч■L∙їсГР$i][Д1ЇЪ№┼|¤ЬdЭ║!][
2ЇЪ* °|∙°ЬdЭUi][neЇЪ)
\(¤oъМ╤!][(|ЇЪ) №
╗u┼¤╠сkl!][]}ЇЪ*№
°
#F
╔ва¤5╓╞3!][PШЇЪ*° в∙сkli][ЧЇЪ)
#ю=╨∙Ў5╓╞3i][Е▌ЇЪ)№{▓У¤\Ё.Щ!][╗▐ЇЪ*°и┤У∙ў\Ё.Щi][щЇЪ)№╟]│¤З╢Н!][7ъЇЪ*°#бyЩ∙З╢Нi][┴¤ЇЪ)№▀M╨¤kL┴#!][√■ЇЪ*°
░єL¤сГР$!]["пїЪ*!° ТїL∙їсГР$i][*╕їЪ)"№""I¤Ц2╛!][-їЪ*°ё$I∙ЎЦ2╛i][═HїЪ)№#х└¤з█!][#JїЪ*° Зпш∙√з█i][ё`їЪ)№AQз¤)ruo!]['bїЪ*°ЄkL┴#ТWз∙ё)ruoi][╘bїЪ+)ruo!][VЮїЪ)№
щcъ¤uвХ╤!][JэїЪ*%° П.∙°oъМ╤i][╬ЎЪ)&№╬~┼¤╠сkl!][ЎЪ*'°x┼∙·╠сkli][6ЎЪ)(№
&!][lЎЪ*)° :eъ∙uвХ
W)I¤Ц2╛!][║│ЎЪ*4°°° Д/I∙єЦ2╛i][g┤ЎЪ+5Ц2╛!][s╧ЎЪ)6№!вш¤з█'!][й╨ЎЪ*7°#╚▒╨∙ўз█'i][ШчЎЪ)8№#М¤)ruo!][щшЎЪ*9°ч\з∙Ї)ruoi][¤$ўЪ):№√юЎ¤фx▄ф%!][3&ўЪ*;°(шЎ∙Ўфx▄ф%i][Т4ўЪ)<№4°L¤сГР&!][╚5ўЪ*=°ч■L∙їсГР&i][╨i][gдўЪ)D№╝йа¤5╓╞3!][ЬеўЪ*E°oпа∙∙5╓╞3i][╥ъўЪ)F№{▓У¤\Ё.Щ&!][ьўЪ*G°и┤У∙Ё\Ё.Щ&i][NЎўЪ)H№╟]│¤З╢Н&!][ДўўЪ*I°[│∙яЗ╢Н&i][
°Ъ)J№▀M╨¤kL┴#!][E
°Ъ*K°
K╨∙їkL┴#i][
AQз¤)ruo !][O!][oo°Ъ*S°з█' i][>n°Ъ)R№№#@Ча¤-оФ!][`°Ъ*M° ╨76∙ї-оФi][+9°Ъ)N№#Ш╫х¤Ц2╛ !][Б:°Ъ*O°ё$I∙ЎЦ2╛ i][V°Ъ)P№
░єL¤сГР!][n╝°Ъ*V° ТїL∙ўсГРi][v┼°Ъ)W№ i][гл°Ъ)T№
!][∙Ъ)\№╬~┼¤╠сkl!][P∙Ъ*]°x┼∙сkli][Г*∙Ъ)^№Ьhъ¤uвХ
!][╕+∙Ъ*_°Onъ∙uвХ
i][e,∙Ъ+`uвХ
MIR S05-154∙ў╓╛ЙО !][3B7∙Ъ*a° dЖG'qД
W)I¤Ц2╛!][┴∙Ъ*i°°yqaP│∙∙З╢Нi][▒Ф∙Ъ)f№v:6¤-оФ!][чХ∙Ъ*g°#dyq∙ё-оФi][╤┐∙Ъ)h№
╔ва¤5╓╞3!][3·!][ЎЧ·Ъ*x°фx▄hs┼∙·╠сklЪ)p№4°i][│▒·Ъ)y№C·Ъ*q°ч■L∙°сГРi][L·Ъ)r№┼|¤ЬdЭU$!][RM·Ъ*s°|∙ёЬdЭU$i][■M·Ъ+tЬdЭU$!][А·Ъ)u№#>b]¤oъМ╤!][\Б·Ъ*v°·%∙·oъМ╤i][┴Ц·Ъ)w№
!][щ▓·Ъ*z° да∙Ў5╓╞3
16¤-оФ!][Н√Ъ*Г°°i]╨76∙є-оФi][xF√Ъ)Д№""I¤Ц2╛*}°и┤У∙Ё\Ё.Щi][Ъ√Ъ)~№╟]│¤З╢!][╨√Ъ*°[│∙З╢i][Z√Ъ)А№
!][оG√Ъ*Е°ё$I∙ЁЦ2╛
AєL¤сГР!][└|√Ъ*Й°з█ТWз∙Ё)ruoi][я╕√Ъ)К№√юЎ¤фx▄ф!][%║√Ъ*Л°(шЎ∙°фx▄фi][Д╚√Ъ)М№
!][║╔√Ъ*Н° ТїL∙∙сГР
i][f╩√Ъ+ОсГР
\(¤oъМ╤i][н№!][т№Ъ*Т° !][├╥√Ъ)П№#е}¤ЬdЭU&!][╘√Ъ*Р° c
#Б│∙°oъМ╤ i][g№Ъ)У№╬~┼¤╠сk!][Ь№Ъ*Ф°x┼∙·╠сki][╧7№Ъ)Х№#C┘ю¤uвХ
!][%9№Ъ*Ц° :eъ∙uвХ
i][A.B№Ъ*Ч°B%ЄGNГ.> 6ь)№№ЫvFb║Y))J
!][:а№Ъ*Э°vЛ№Ъ*Ы° aP│∙╢Нi][Я№Ъ)Ь№▀M╨¤kL┴# ЫH╜T╤▓_цФ~∙▄╓╛ЙО'i][─~№Ъ)Ш№
i][¤б№Ъ)Ю№v:6¤-оФ
Hello jpitt,
In the previous message, I inserted the result after entering the command " set term vtnt"
With other types, too, nothing happened.
I get the same result on a computer that is located in the subnet 192.168.3.
Nothing has changed with Putty either.
Hi Alexandr,
The character encoding obviously looks wrong. These links might help in trying to change that:
https://superuser.com/questions/1121273/what-encoding-does-ms-windows-telnet-use-by-default
https://documentation.help/PuTTY/config-charset.html
Your earlier screenshot shows the operating system language is set to Russian, I wonder if that is interfering with the telnet connections.
Thank you,
jpitt