The Thunderboard Forum is no longer active. If you would like to post a question regarding Thunderboard Kits, please use the Bluetooth Forum.

Forum

    To receive email updates about this thread, click the Follow button and select Email Subscriptions at the top of the thread page.
    • Tips for troubleshooting and asking questions

      tmonte | 08/217/2019 | 04:14 AM

      1. Clarify to yourself what the specific issue is.

      2. Apply basic troubleshooting:

      • Check hardware connections with multimeter.
      • Use logic analyzers/oscilloscopes.
      • Use Simplicity Studio Debugger/Energy Profiler/Network Analyzer/BG Tool, use logging prints.

      3. Consult the datasheets and reference manuals. Sources include:

      4. Search to see if someone has asked the same question already.

      5. Include the relevant parts of your development setup in the problem description. Examples include:

      • SDK version
      • Part number
      • Radio board vs custom hardware
      • Host OS
      • Mobile phone model and OS version
      • Compiler and compiler version

      6. Include steps to reproduce the problem or specific conditions the problem occurs in.

      7. Be patient and avoid making duplicates of your question.

      For general community usage please refer to the Silicon Labs Community Guidelines.

      • Discussion Forums
      • Thunderboard Kits
      0
      Replies
      Unanswered
    • Analog signal read

      Filippo Cinotti | 07/203/2020 | 07:30 AM
      Good morning, I am new with thunderboard BG22, and I am trying to convert a simple arduino code into a project with bg22. The aim is really simple... I have to read analog signal coming from a wearable force sensor and do some simple data elaboration with it. However, the enviroment is new and I have some difficulties in finding the way to do that... could you suggest me some tutorial/ give me some hints on how to do this? Thanks in advance, Filippo
      • Discussion Forums
      • Thunderboard Kits
      0
      Replies
      Unanswered
    • Cannot get the BG22 Thunderboard to send keycodes using the HID over GATT service

      Anthony Dobaj | 07/186/2020 | 11:09 PM
      Although I can connect the Thunderboard to either an iOS or Android device they never receive any of the keycodes I send. Here is the code to send the character.
      	hidTempBuffer[2] = 0x08;
          gecko_cmd_gatt_server_send_characteristic_notification(0xFF, gattdb_report, length, hidTempBuffer);
          hidTempBuffer[2] = 0;
          gecko_cmd_gatt_server_send_characteristic_notification(0xFF, gattdb_report, length, hidTempBuffer);
      

      Here is the gatt.xml file:

      <?xml version="1.0" encoding="UTF-8" standalone="no"?>
      <!--Custom BLE GATT-->
      <gatt gatt_caching="true" generic_attribute_service="true" header="gatt_db.h" name="Custom BLE GATT" out="gatt_db.c" prefix="gattdb_">
        
        <!--Device Information-->
        <service advertise="false" id="device_information" name="Device Information" requirement="mandatory" sourceId="org.bluetooth.service.device_information" type="primary" uuid="180A">
          <informativeText>Abstract: The Device Information Service exposes manufacturer and/or vendor information about a device. Summary: This service exposes manufacturer information about a device. The Device Information Service is instantiated as a Primary Service. Only one instance of the Device Information Service is exposed on a device. </informativeText>
          
          <!--PnP ID-->
          <characteristic id="pnp_id" name="PnP ID" sourceId="org.bluetooth.characteristic.pnp_id" uuid="2A50">
            <informativeText>Custom characteristic</informativeText>
            <value length="7" type="hex" variable_length="false">0x014700ffffffff</value>
            <properties const="true" const_requirement="optional" indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="false" write_no_response_requirement="excluded" write_requirement="excluded"/>
          </characteristic>
          
          <!--Manufacturer Name String-->
          <characteristic id="manufacturing_name_string" name="Manufacturer Name String" sourceId="org.bluetooth.characteristic.manufacturer_name_string" uuid="2A29">
            <informativeText>Abstract: The value of this characteristic is a UTF-8 string representing the name of the manufacturer of the device. </informativeText>
            <value length="3" type="utf-8" variable_length="false">AST</value>
            <properties indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="false" write_requirement="excluded"/>
          </characteristic>
          
          <!--Model Number String-->
          <characteristic id="model_number_string" name="Model Number String" sourceId="org.bluetooth.characteristic.model_number_string" uuid="2A24">
            <informativeText>Abstract: The value of this characteristic is a UTF-8 string representing the model number assigned by the device vendor. </informativeText>
            <value length="1" type="utf-8" variable_length="false">1</value>
            <properties indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="false" write_no_response_requirement="excluded" write_requirement="excluded"/>
          </characteristic>
          
          <!--System ID-->
          <characteristic id="system_id" name="System ID" sourceId="org.bluetooth.characteristic.system_id" uuid="2A23">
            <informativeText>Abstract: The SYSTEM ID characteristic consists of a structure with two fields. The first field are the LSOs and the second field contains the MSOs.       This is a 64-bit structure which consists of a 40-bit manufacturer-defined identifier concatenated with a 24 bit unique Organizationally Unique Identifier (OUI). The OUI is issued by the IEEE Registration Authority (http://standards.ieee.org/regauth/index.html) and is required to be used in accordance with IEEE Standard 802-2001.6 while the least significant 40 bits are manufacturer defined.       If System ID generated based on a Bluetooth Device Address, it is required to be done as follows. System ID and the Bluetooth Device Address have a very similar structure: a Bluetooth Device Address is 48 bits in length and consists of a 24 bit Company Assigned Identifier (manufacturer defined identifier) concatenated with a 24 bit Company Identifier (OUI). In order to encapsulate a Bluetooth Device Address as System ID, the Company Identifier is concatenated with 0xFFFE followed by the Company Assigned Identifier of the Bluetooth Address. For more guidelines related to EUI-64, refer to http://standards.ieee.org/develop/regauth/tut/eui64.pdf. Examples: If the system ID is based of a Bluetooth Device Address with a Company Identifier (OUI) is 0x123456 and the Company Assigned Identifier is 0x9ABCDE, then the System Identifier is required to be 0x123456FFFE9ABCDE. </informativeText>
            <value length="6" type="hex" variable_length="false">000102030405</value>
            <properties const="true" const_requirement="optional" read="true" read_requirement="optional"/>
          </characteristic>
        </service>
        
        <!--Generic Access-->
        <service advertise="true" name="Generic Access" requirement="mandatory" sourceId="org.bluetooth.service.generic_access" type="primary" uuid="1800">
          <informativeText>Abstract: The generic_access service contains generic information about the device. All available Characteristics are readonly. </informativeText>
          
          <!--Device Name-->
          <characteristic id="device_name" name="Device Name" sourceId="org.bluetooth.characteristic.gap.device_name" uuid="2A00">
            <informativeText/>
            <value length="6" type="utf-8" variable_length="false">gestr4</value>
            <properties read="true" read_requirement="optional" write="true" write_requirement="optional"/>
          </characteristic>
          
          <!--Appearance-->
          <characteristic name="Appearance" sourceId="org.bluetooth.characteristic.gap.appearance" uuid="2A01">
            <informativeText>Abstract: The external appearance of this device. The values are composed of a category (10-bits) and sub-categories (6-bits). </informativeText>
            <value length="2" type="hex" variable_length="false">0000</value>
            <properties const="true" const_requirement="optional" read="true" read_requirement="optional"/>
          </characteristic>
        </service>
        
        <!--Silicon Labs OTA-->
        <service advertise="false" name="Silicon Labs OTA" requirement="mandatory" sourceId="com.silabs.service.ota" type="primary" uuid="1D14D6EE-FD63-4FA1-BFA4-8F47B42119F0">
          <informativeText>Abstract: The Silicon Labs OTA Service enables over-the-air firmware update of the device. </informativeText>
          
          <!--Silicon Labs OTA Control-->
          <characteristic id="ota_control" name="Silicon Labs OTA Control" sourceId="com.silabs.characteristic.ota_control" uuid="F7BF3564-FB6D-4E53-88A4-5E37E0326063">
            <informativeText>Abstract: Silicon Labs OTA Control. </informativeText>
            <value length="1" type="user" variable_length="false"/>
            <properties write="true" write_requirement="optional"/>
          </characteristic>
        </service>
        
        <!--Battery Service-->
        <service advertise="false" id="battery_service" name="Battery Service" requirement="mandatory" sourceId="org.bluetooth.service.battery_service" type="primary" uuid="180F">
          <informativeText>Abstract:  The Battery Service exposes the state of a battery within a device.  Summary:  The Battery Service exposes the Battery State and Battery Level of a single battery or set of batteries in a device.  </informativeText>
          
          <!--Battery Level-->
          <characteristic id="battery_level" name="Battery Level" sourceId="org.bluetooth.characteristic.battery_level" uuid="2A19">
            <informativeText>Abstract:  The current charge level of a battery. 100% represents fully charged while 0% represents fully discharged.  </informativeText>
            <value length="1" type="hex" variable_length="false"/>
            <properties indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="optional" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="false" write_no_response_requirement="excluded" write_requirement="excluded"/>
            
            <!--Characteristic Presentation Format-->
            <descriptor id="characteristic_presentation_format" name="Characteristic Presentation Format" sourceId="org.bluetooth.descriptor.gatt.characteristic_presentation_format" uuid="2904">
              <properties read="true" read_requirement="mandatory" write="false" write_requirement="excluded"/>
              <value length="7" type="hex" variable_length="false"/>
            </descriptor>
            
            <!--Client Characteristic Configuration-->
            <descriptor id="client_characteristic_configuration" name="Client Characteristic Configuration" sourceId="org.bluetooth.descriptor.gatt.client_characteristic_configuration" uuid="2902">
              <properties read="true" read_requirement="mandatory" write="true" write_requirement="mandatory"/>
              <value length="2" type="hex" variable_length="false"/>
            </descriptor>
          </characteristic>
        </service>
        
        <!--Scan Parameters-->
        <service advertise="false" id="scan_parameters" name="Scan Parameters" requirement="mandatory" sourceId="org.bluetooth.service.scan_parameters" type="primary" uuid="1813">
          <informativeText>Abstract:  This service enables a GATT Client to store the LE scan parameters it is using on a GATT Server device so that the GATT Server can  utilize the information to adjust behavior to optimize power consumption and/or reconnection latency  Summary:  The Scan Parameters Service enables a GATT Server device to expose a characteristic for the GATT Client to write its scan interval and scan window on the GATT Server device.  </informativeText>
          
          <!--Scan Interval Window-->
          <characteristic id="scan_interval_window" name="Scan Interval Window" sourceId="org.bluetooth.characteristic.scan_interval_window" uuid="2A4F">
            <informativeText>Abstract:  The Scan Interval Window characteristic is used to store the scan parameters of the GATT Client. Included in this characteristic are the Scan Interval and Scan Window of the GATT Client device.  Summary:  The Scan Interval Window characteristic is used to store the scan parameters of the GATT Client.  The GATT Server can use these values to optimize its own advertisement rate and to minimize      the rate of its own advertisements while also minimizing the latency of reconnections.  </informativeText>
            <value length="4" type="hex" variable_length="false"/>
            <properties indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="false" read_requirement="excluded" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="true" write_no_response_requirement="mandatory" write_requirement="excluded"/>
          </characteristic>
          
          <!--Scan Refresh-->
          <characteristic id="scan_refresh" name="Scan Refresh" sourceId="org.bluetooth.characteristic.scan_refresh" uuid="2A31">
            <informativeText>Abstract:  The Scan Refresh characteristic is used to notify the Client that the Server requires the Scan Interval Window characteristic to be written with the latest values upon notification.  </informativeText>
            <value length="1" type="hex" variable_length="false"/>
            <properties indicate="false" indicate_requirement="excluded" notify="true" notify_requirement="mandatory" read="false" read_requirement="excluded" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="false" write_no_response_requirement="excluded" write_requirement="excluded"/>
            
            <!--Client Characteristic Configuration-->
            <descriptor id="client_characteristic_configuration_3" name="Client Characteristic Configuration" sourceId="org.bluetooth.descriptor.gatt.client_characteristic_configuration" uuid="2902">
              <properties read="true" read_requirement="mandatory" write="true" write_requirement="mandatory"/>
              <value length="2" type="hex" variable_length="false"/>
            </descriptor>
          </characteristic>
        </service>
        
        <!--Human Interface Device-->
        <service advertise="true" id="human_interface_device" name="Human Interface Device" requirement="mandatory" sourceId="org.bluetooth.service.human_interface_device" type="primary" uuid="1812">
          <informativeText>Abstract:  This service exposes the HID reports and other HID data intended for HID Hosts and HID Devices.  Summary:  The HID Service exposes characteristics required for a HID Device to transfer HID report descriptors and reports to a HID Host. This also exposes the characteristics for a HID Host to write to a Device. The Human Interface Device Service is instantiated as a Primary Service.  </informativeText>
          <include id="battery_service"/>
          
          <!--Protocol Mode-->
          <characteristic id="protocol_mode" name="Protocol Mode" sourceId="org.bluetooth.characteristic.protocol_mode" uuid="2A4E">
            <informativeText>Summary:  The Protocol Mode characteristic is used to expose the current protocol mode of the HID Service with which it is associated, or to set the desired protocol mode of the HID Service.  </informativeText>
            <value length="1" type="hex" variable_length="false">1</value>
            <properties indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="true" write_no_response_requirement="mandatory" write_requirement="excluded"/>
          </characteristic>
          
          <!--Report-->
          <characteristic id="report" name="Report" sourceId="org.bluetooth.characteristic.report" uuid="2A4D">
            <informativeText>Abstract:  The Report characteristic is used to exchange data between a HID Device and a HID Host.  Summary:  The Report characteristic value contains Input Report, Output Report or Feature Report data to be transferred between the HID Device and HID Host.  </informativeText>
            <value length="8" type="hex" variable_length="false">0x0000000000000000</value>
            <properties const="true" const_requirement="optional" indicate="false" indicate_requirement="excluded" notify="true" notify_requirement="mandatory" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="true" write_no_response="false" write_no_response_requirement="excluded" write_requirement="optional"/>
            
            <!--Client Characteristic Configuration-->
            <descriptor id="client_characteristic_configuration" name="Client Characteristic Configuration" sourceId="org.bluetooth.descriptor.gatt.client_characteristic_configuration" uuid="2902">
              <properties encrypted_read="true" encrypted_read_requirement="mandatory" encrypted_write="true" encrypted_write_requirement="mandatory"/>
              <value length="2" type="hex" variable_length="false"/>
            </descriptor>
            
            <!--Report Reference-->
            <descriptor id="report_reference" name="Report Reference" sourceId="org.bluetooth.descriptor.report_reference" uuid="2908">
              <properties const="true" const_requirement="optional" encrypted_read="true" encrypted_read_requirement="mandatory" read="true" read_requirement="optional" write="false" write_requirement="excluded"/>
              <value length="11" type="hex" variable_length="true">0001</value>
            </descriptor>
          </characteristic>
          
          <!--Report Map-->
          <characteristic id="report_map" name="Report Map" sourceId="org.bluetooth.characteristic.report_map" uuid="2A4B">
            <informativeText>Summary:  The Report Map characteristic is used to define formatting information for Input Report, Output Report, and Feature Report data transferred between a HID Device and HID Host, information on how this data can be used, and other information regarding physical aspects of the device (i.e. that the device functions as a keyboard, for example, or has multiple functions such as a keyboard and volume controls).       Only a single instance of this characteristic exists as part of a HID Service.  </informativeText>
            <value length="45" type="hex" variable_length="false">05010906A101050719E029E71500250175019508810295017508810195057501050819012905910295017503910195067508150025650507190029658100C0</value>
            <properties encrypted_read="true" encrypted_read_requirement="mandatory" indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="false" write_no_response_requirement="excluded" write_requirement="excluded"/>
            
            <!--External Report Reference-->
            <descriptor id="external_report_reference" name="External Report Reference" sourceId="org.bluetooth.descriptor.external_report_reference" uuid="2907">
              <properties read="true" read_requirement="mandatory" write="false" write_requirement="excluded"/>
              <value length="2" type="hex" variable_length="false"/>
            </descriptor>
          </characteristic>
          
          <!--HID Information-->
          <characteristic id="hid_information" name="HID Information" sourceId="org.bluetooth.characteristic.hid_information" uuid="2A4A">
            <informativeText>Abstract:  The HID Information Characteristic returns the HID attributes when read.  Summary:  The HID Information Characteristic contains the HID attributes.  The value of this Characteristic is static and can be cached for the lifetime of the bond between the HID device and the HID host.  </informativeText>
            <value length="4" type="hex" variable_length="false">01110002</value>
            <properties indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="true" read_requirement="mandatory" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="false" write_no_response_requirement="excluded" write_requirement="excluded"/>
          </characteristic>
          
          <!--HID Control Point-->
          <characteristic id="hid_control_point" name="HID Control Point" sourceId="org.bluetooth.characteristic.hid_control_point" uuid="2A4C">
            <informativeText>Summary:  The HID Control Point characteristic is a control-point attribute that defines the following HID Commands when written:             - Suspend ( Refer to Section 7.4.2, Bluetooth HID Profile Specification 1.0             - Exit Suspend (Refer to Section 7.4.2, Bluetooth HID Profile Specification 1.0  </informativeText>
            <value length="1" type="hex" variable_length="false">00</value>
            <properties indicate="false" indicate_requirement="excluded" notify="false" notify_requirement="excluded" read="false" read_requirement="excluded" reliable_write="false" reliable_write_requirement="excluded" write="false" write_no_response="true" write_no_response_requirement="mandatory" write_requirement="excluded"/>
          </characteristic>
        </service>
      </gatt>
      

      What is missing here?

      • Discussion Forums
      • Thunderboard Kits
      0
      Replies
      Unanswered
    • HID Game Controller

      James Carruthers | 06/174/2020 | 09:33 PM

      Hi all,

       

      Can anyone give me a point in the right direction for creating a HID game controller with the board?

       

       

      James

       

      • Discussion Forums
      • Thunderboard Kits
      6
      Replies
      Unanswered
    • Thunderboard and external sensor

      qingyu lin | 06/177/2020 | 10:41 PM

      I'm still new to Simplicity Studio and thunderboard. I'm trying to figure out how to program the thunderboard and let it get reading from the external sensor and print out the reading. 

      1. is there a detailed tutorial that also explains what to do on simplicity studio 

      2. is it similar to arudino ( like i can just flash the file and it does everything)

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      1
      Replies
      Answered
    • Thunderboard EFR32BG22 current consumption

      Clarck_D | 05/150/2020 | 10:16 AM

      Hi all,

       

      I'm trying to measure how much current my board draw in EM2 and EM4 mode. I've disabled all the peripherals but I can't get better than 300µA in any mode. I would expect to have much less for the EM4 mode but I don't see any difference right now.

       

      I'm powering my board through the pins EXP20 and EXP1. I'm using the soc-thunderboard example and here is the changes I've made to it :

       

      This is my last test before we can choose which product we'll use, thanks in advance for your help  :)

       

      • Discussion Forums
      • Thunderboard Kits
      13
      Replies
      Unanswered
    • My Thunderboard cannot get into debug mode with "DP write failed".

      hxin | 06/157/2020 | 07:15 PM

      Hi There,

      Today when I tried some test programs from github, my thunderboard could not get into debug mode with this error message:

      Did some searchings online, I tried to recover the device but also failed as:

      Any idea about this problem, I appriaciate it.

      From the Simplicity studio, the device is still recognized normally as Thunderboard EFR32GB22(BRD4184A Rev A01). My simplicity studio is SV4.1.13.5.

      Thanks,

      Henry

      • Discussion Forums
      • Thunderboard Kits
      2
      Replies
      Unanswered
    • EFR32BG22C222F352GM32 debugging issue

      Moumita Kundu | 06/171/2020 | 10:47 AM

      To program/debug EFR32BG22C222F352GM32 do we need PTI DATA and PTI FRAME? Why the PTI DATA , PTI FRAME, TX , RX connections are given in the 10 pin programming connector?

      If we use one 6 pin like VDD, VSS, RST, SWO, SWDIO, and SWCLK for programming/debugging purpose then wha will the problems we have to face, please guide me I am confused.

      Can't we use separately these  PTI DATA , PTI FRAME, TX , RX connections?

      • Discussion Forums
      • Thunderboard Kits
      1
      Replies
      Unanswered
    • Problem in receiving string UART

      Nabil DRISSI EL BOUZAIDI | 06/169/2020 | 12:29 PM

      Hi,

      I'm using the Thunderboard BG22 and I have some problem to receive data with the UART, I can just receive 2 characters as shown in picture below :

       

      so in com7 there is the string that I need to receive but I could just receive the 2 first 2 characters of it,

      I was thinking if I need to add a delay, but I don't know how

      This is the code that I use

      
      void sendData(USART_TypeDef *usart, uint8_t data[]){
      	int i;
      	for (i = 0; i <strlen(data) ; i++){
      		USART_Tx(usart, data[i]);
      	}
      	USART_Tx(USART1, '\r');
      }
      
      static volatile char recv[10];
      static volatile char C;
      
      
      int main(void)
      {
        uint32_t i;
      
        // Chip errata
        CHIP_Init();
      
        // Initialize GPIO and USART1
        initCmu();
        initGpio();
        initUsart1();
        USART_BaudrateAsyncSet(USART1,0,9600,usartOVS16);
      
        int j;
        while (1)
        {
      	  uint8_t buff[8] = "AT$I=10\r";
      	  sendData(USART1, buff);
      	  for (j = 0 ; j < 10 ; j++){
      	  			  C = USART_Rx(USART1);
      	  			  if (C != '\r')
      	  				recv[j] = C;
      	  }
        }
      }

       

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      6
      Replies
      Answered
    • BOM for Thunderboard SLTB010A

      Nishant Bhaskar | 06/170/2020 | 12:35 AM

      Hi,

      I am looking for the BOM for the Thunderboard SLTB010A. In particular I am looking for the part number for the HFXO 38.4 MHz oscillator on board. I tried checking on Simplicity Studio, but couldn't find an exact BOM.

      Thanks 

      Nishant

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      1
      Replies
      Answered
    • Problem with the USART in Thunderboard EFR32BG22

      Nabil DRISSI EL BOUZAIDI | 06/167/2020 | 07:42 AM

      Hi,

      I'm using the USART of the Thunderboard EFR32BG22, is it normal that when I use "Printf" or "PrintLog" fonctions in my code the USART send the data ?

      I also have a problem I can't send data using the USART_TX fonctions.

      • Discussion Forums
      • 32-bit MCUs
      • Answered
      13
      Replies
      Answered
    • Thunderboard EFR32BG22 (SLTB010A) Example Problem

      Fatih ÇEKEN | 04/117/2020 | 04:35 PM

      Hi, I'm dealing with Thunderboard for BG22 (SLTB010A-BRD4184A). This is first experience with Silicon Labs device and Simplicity Studio.

      I tested board with default firmware with Android app, there is no problem.

      Now, I want to test simple Soc-iBeacon example. However I have got error, the screenshot is below. 

      Also, I can't see any examples in "Getting Started" tab. 

      GNU ARM v7.2.1

      Bluetooth SDK v2.13.4.0

       

       

      Thank you.

      • Discussion Forums
      • Thunderboard Kits
      14
      Replies
      Unanswered
    • Thunderboard EFR32BG22 VCOM disable

      Neil Wilson | 05/142/2020 | 09:49 PM

      From my understanding of the schematic the EFR32BG22 USART1 goes to the on-board debugger and is presented as a VCOM UART - the pins are also wired to the Simplicity connector as SI_UART.

      Is it possible to disable the VCOM UART so that I can use the Simplicity connector to connect to some other hardware I have to USART1 ?

      If it means adding a wire or removing a resistor or some other small mod then I am happy to make that.

      BTW I would still like to keep the USB debug connection for the JLINK loading/debugging if possible.

      Thanks.

      • Discussion Forums
      • Thunderboard Kits
      2
      Replies
      Unanswered
    • Thunderboard BG22 I2C and app

      qingyu lin | 06/164/2020 | 05:36 PM

      I'm looking to purchase thunderboard BG22, but i have a few question

      1. how difficult is it to implement i2c sensor, I was only able to one sample code (from silicon lab github). From the look of it, i2c implementation is a little different from using Wire.h.

      2. does the thunderboard app show external sensor data or just built-in sensor data on the board

        

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      1
      Replies
      Answered
    • Android Thunderboard App fails to find any device on Samsung Galaxy A20

      Roya Dibaj | 06/160/2020 | 12:57 PM

      Hi,

      Thunderboard App fails to find SLTB010A or any other SiLabs device on Samsung Galaxy A20. All permissions including the location are given. Please help resolve this issue.

       

      • Discussion Forums
      • Thunderboard Kits
      • Answered
      4
      Replies
      Answered