I have a custom board with a bgm13s module that currently outputs logging info out a serial port via printf. When this board is mounted in the device I am unable to get access to the uart pins to connect a serial to USB cable to my laptop. Is there something I can setup to get this serial data sent over ble using the custom boards bgm13 module (no hardware changes allowed) so that I can view and save the log output on my android tablet/phone or pc laptop?
Bgm13s serial printf equivalent over ble
I have a custom board with a bgm13s module that currently outputs logging info out a serial port via printf. When this board is mounted in the device I am unable to get access to the uart pins to connect a serial to USB cable to my laptop. Is there something I can setup to get this serial data sent over ble using the custom boards bgm13 module (no hardware changes allowed) so that I can view and save the log output on my android tablet/phone or pc laptop?
https://docs.silabs.com/bluetooth/2.13/code-examples/applications/spp-serial-port-profile-over-ble