QuickSense™ Touchless Slider 2 Evaluation Kit
IrSlider2EK
The Si1140 Infrared Slider Demo is a Silicon Labs patent-pending infrared touchless slider technique. This innovative touchless slider boasts excellent range, visible LED tracking, and both swipe and set gesture recognition. The USB-powered demonstration is controlled by an ultra-low-power Silicon Labs C8051F800 MCU and incorporates an Si1142, two infrared LEDs and eight visible LEDs. The QuickSense Studio development environment supports this unique demonstration board with a powerful performance analysis tool that enables real-time reflectivity monitoring.
See the IrSlider2EK board in action
Click to Buy
The IrSlider2EK includes the following items:
Additional IrSliderEK resources:
QuickSense™ Touchless Slider Evaluation Kit
IrSliderEK
TheSi1120 Infrared Slider Demo is a Silicon Labs patent-pending infrared touchless slider technique. This innovative touchless slider boasts excellent range, visible LED tracking, and both swipe and set gesture recognition. The USB-powered demonstration is controlled by an ultra-low-power Silicon Labs C8051F900 MCU and incorporates an Si1120 proximity and ambient light sensor IC, two infrared LEDs and eight visible LEDs. The QuickSense Studio development environment supports this unique demonstration board with a powerful performance analysis tool that enables real-time reflectivity monitoring.
Click to Buy