The CP210x USB to UART Bridge Virtual COM Port (VCP) drivers are required for device operation as a Virtual COM Port to facilitate host communication with CP210x products. These devices can also interface to a host using the USBXpress direct access driver.
Download for Windows 2000/XP/Server 2003/Vista (v5.2.2) * The CP210x Manufacturing DLL and Runtime DLL have been updated and must be used with v5.0 and later of the CP210x Windows VCP Driver. Application Note Software downloads affected are AN144SW.zip, AN197SW.zip, AN205SW.zip and AN223SW.zip.
Download for Macintosh OSX Download for Macintosh OS9 Download for Linux 2.6 Download for Linux 2.4
|