Sign in to mysilabs.com

Username: 
Password: 
Not a member? Sign up today
Forgot password? Click here

8051 Microcontrollers - USB ToolStick

USB ToolStick

ToolStick-EK


Documents
   User's Guide
 Credit Card Shopping 
  Add to Cart
 

The ToolStick evaluation platform is a fully contained evaluation system in a USB stick that demonstrates Silicon Laboratories' easy-to-use development tools. 

Using only a PC with a USB port, designers can fully experience the Silicon Laboratories software development environment in conjunction with the on-chip debugging hardware that allows full, non-intrusive access to the C8051F mixed-signal MCUs CPU, peripherals and memory. The target microcontroller on the board is a Silicon Laboratories C8051F300 which interfaces with the PC via the integrated Silicon Laboratories USB debug adapter that uses the C8051F321 USB MCU. The software development environment consists of the easy–to-use Integrated Development Environment (IDE), editor, debugger, Flash programmer as well as a demonstration version of the Keil compiler.

The ToolStick kit contains the following items:


 
 

back to top