Sign in to mysilabs.com

Username: 
Password: 
Not a member? Sign up today
Forgot password? Click here

Mixed-Signal ICs - USB ToolStick

 

The Silicon Labs ToolStick is an easy to use development system that allows designers to develop and debug application firmware directly on the target microcontroller using the Silicon Labs Integrated Development Environment (IDE). Once complete, designers can replace the Daughter Card with a Programming Adapter and program blank devices for use in their actual system.

Base Adapter
The Base Adapter connects to the PC using a USB connector and supports any Daughter Card or Programming Adapter.

Daughter Card
The target MCU and application circuitry are located on the Daughter Card; the IDE interfaces with this MCU. The Daughter Card plugs into the Base Adapter.

Programming Adapter
The Programming Adapter provides the appropriate mechanical socket to program a blank device. The Programming Adapter plugs into the Base Adapter.

Software
The required software to debug on the ToolStick development platform is available as free downloads
ToolStick Development Tools – includes example code, documentation and the ToolStick Terminal application
Silicon Laboratories IDE – integrates a source-code editor, source-level debugger and an in-system Flash programmer
Keil Evaluation 8051 Tools – includes an evaluation version of the Keil 8051 assembler, compiler and linker
Production Programmer – use with the Programming Adapters to easily program devices for prototypes or production

Install the ToolStick Development Tools and Silicon Labs IDE to the same directory and follow the appropriate Daughter Card User’s Guide for instructions on using the development tools and running the demonstration firmware.

Getting Started
The easiest way to get started experimenting with the ToolStick is with the ToolStick Starter Kit. This kit is a complete development system that contains a ToolStick Base Adapter and an interchangeable C8051F330 MCU Daughter Card. To continue developing with a selected MCU, use the guide below to choose the appropriate Daughter Card and Programming Adapter. Daughter Cards are sold individually and require a separate Base Adapter to be purchased if not previously owned. Programming Adapter kits include a Base Adapter and a separate purchase is not required.

ToolStick Starter Kit ($24.99)

See the Silicon Labs MCUniversity page for information on ToolStick solutions for colleges and universities. See the the Capacitive Touch Sense page for information on Silicon Labs' touch sense solution and ToolStick development boards.

To develop with a different MCU, designers need the Base Adapter and the selector guide below to choose the appropriate Daughter Card and Programming Adapter.

Part Number ToolStick Base Adapter ($17.50) ToolStick Daughter Card ($9.90) ToolStick Programming Adapter ($69)
C8051F300/301/302/303/304/305 TOOLSTICKBA
ToolStick300DC
 User's Guide
 ToolStick300PP
 User's Guide
C8051F310/312/314 TOOLSTICKBA
ToolStick311DC
 User's Guide
ToolStick310PP
User's Guide
C8051F311/313/315 TOOLSTICKBA
ToolStick311DC
 User's Guide
ToolStick311PP
User's Guide
C8051F316/317 TOOLSTICKBA
ToolStick311DC
 User's Guide
ToolStick316PP
User's Guide
C8051F320 TOOLSTICKBA
ToolStick321DC
 User's Guide
ToolStick320PP
User's Guide
C8051F321 TOOLSTICKBA
ToolStick321DC
 User's Guide
ToolStick321PP
User's Guide
C8051F326 TOOLSTICKBA
ToolStick327DC
 User's Guide
ToolStick326PP
User's Guide
C8051F327 TOOLSTICKBA
ToolStick327DC
 User's Guide
ToolStick321PP
User's Guide
C8051F330/331/332/333/334/335 TOOLSTICKBA
ToolStick330DC
 User's Guide
ToolStick330PP
 User's Guide
C8051F336/337 TOOLSTICKBA
ToolStick336DC
 User's Guide
ToolStick330PP
User's Guide
C8051F338/339 TOOLSTICKBA
ToolStick336DC
 User's Guide
ToolStick316PP
User's Guide
C8051F340/341/344/345 TOOLSTICKBA
ToolStick342DC
 User's Guide
ToolStick340PP
User's Guide
C8051F342/343/346/347 TOOLSTICKBA
ToolStick342DC
 User's Guide
ToolStick320PP
User's Guide
C8051F360/363 TOOLSTICKBA
ToolStick360DC
 User's Guide
ToolStick360PP
User's Guide
C8051F361/364/366/368 TOOLSTICKBA
ToolStick360DC
 User's Guide
ToolStick310PP
User's Guide
C8051F362/365/367/369 TOOLSTICKBA
ToolStick360DC
User's Guide
ToolStick311PP
User's Guide
C8051F410/412 TOOLSTICKBA
ToolStick411DC
 User's Guide
ToolStick410PP
User's Guide
C8051F411/413 TOOLSTICKBA
ToolStick411DC
 User's Guide
ToolStick411PP
User's Guide
C8051F520A/521A/523A/524A/526A/527A TOOLSTICKBA
ToolStick530ADC
 User's Guide
ToolStick520PP
User's Guide
C8051F530A/531A/533A/534A/536A/537A-IM TOOLSTICKBA
ToolStick530ADC
 User's Guide
ToolStick530MPP
User's Guide
C8051F530A/531A/533A/534A/536A/537A-IT TOOLSTICKBA
ToolStick530ADC
User's Guide
ToolStick530TPP
User's Guide
C8051F920/930-GM TOOLSTICKBA
ToolStick931DC
User's Guide
ToolStick930MPP
User's Guide
C8051F920/930-GQ TOOLSTICKBA
ToolStick931DC
User's Guide
ToolStick930QPP
User's Guide
C8051F921/931 TOOLSTICKBA
ToolStick931DC
User's Guide
ToolStick931PP
User's Guide
C8051F931 TOOLSTICKBA
CapTouchSenseDC
User's Guide
N/A

ToolStick Accessories and Resources

ToolStick Daughter Card Template
Create a ToolStick compatible Daughter Card using the ToolStick Daughter Card Template. The template includes a schematic, bill of materials and fab drawing for easy development of a ToolStick compatible Daughter Card.

ToolStick Evaluation Kit
The ToolStick Evaluation Kit provides an easy way to evaluate the Silicon Laboratories IDE and the on-chip debug capabilities of our microcontrollers. The target microcontroller on the board is a Silicon Laboratories C8051F300 which interfaces with the PC via the integrated Silicon Laboratories USB Debug Adapter that uses the C8051F321 USB MCU.

ToolStick Evaluation Kit ($10.99)
User's Guide

ToolStick Debug Adapter
The ToolStick Debug Adapter, in conjunction with a ToolStick Base Adapter, provides an interface between the PC’s USB port and the target device’s in-system debug/programming circuitry. The ToolStick Debug Adapter can be used to program and debug a standard Silicon Laboratories MCU development board.

ToolStick Debug Adapter ($8.90)
User's Guide



 

back to top