Choosing the Best RTOS For IoT Development

Choosing the Right RTOS Today Requires Balancing Security, Flexibility, and Ecosystem

05/20/2026 | Sai Ananya Tungaturthi | 3 Min Read

Choosing a real-time operating system (RTOS) was once considered a low-level engineering decision. Tools were selected based on processing, synchronization, or other performance features and it was something that would stay mostly out of sight for the end user. But today, this is no longer a narrow technical decision. Software is now central to how embedded systems are built and choosing an RTOS is foundational to IoT product development. The RTOS you select influences not just scheduling and memory management, but how easily your IoT device connects, how securely it operates, and how quickly your team can move from concept to deployment.


How Do You Choose an RTOS in Embedded Systems?

Developers evaluating Zephyr vs FreeRTOS today are navigating a broader and more complex RTOS landscape than ever. Established options like FreeRTOS continue to be widely used, particularly in cost-sensitive and resource-constrained designs. At the same time, commercial RTOS offerings still appeal to teams that value dedicated support and tightly controlled environments. Alongside these familiar choices, newer open-source platforms such as Zephyr have gained traction by offering a more integrated and scalable approach to modern embedded development.


Zephyr vs FreeRTOS vs Proprietary RTOS Solutions

Each of these reflect a different philosophy. FreeRTOS is a strong choice for simple applications where minimal overhead and familiarity matter most. Its lightweight footprint and large install base make it dependable, but developers often find themselves assembling additional components, connectivity stacks, security features, and middleware, to meet the needs of today’s connected devices.

Proprietary RTOS solutions, on the other hand, tend to offer tightly integrated ecosystems with vendor-specific optimizations. These can reduce initial development effort, especially in highly specialized applications. However, they may introduce long-term constraints around portability, flexibility, and ecosystem dependence, factors that become more significant as product lines scale or evolve.

Zephyr RTOS enters this landscape with a different proposition. As an open-source RTOS backed by the Linux Foundation, it emphasizes modularity, scalability, and built-in support for modern connectivity standards. Instead of treating networking and security as add-ons, Zephyr integrates them into the core platform. This approach aligns well with current IoT requirements, where protocols like Bluetooth Low Energy (LE), Matter, and Thread are increasingly central to product design.


RTOS for IoT Devices Need Security and Scalability

Security has become a defining factor in RTOS selection. With growing regulatory pressure and heightened awareness of device vulnerabilities, developers are looking beyond basic protection. They need support for secure boot, hardware-backed key storage, and resistance to physical and side-channel attacks. While most RTOS options can be extended to include these features, the level of integration, and the effort required to achieve it, varies significantly.

Another important shift is the need for scalability across product portfolios. Many teams are no longer building a single IoT device, but a range of products with shared architecture. In this context, RTOS that can scale from low-power microcontrollers to more capable edge devices without major rework offers a clear advantage.


Silicon Labs’ Simplicity SDK for Zephyr

This is where Silicon Labs’ Simplicity SDK for Zephyr can help. This SDK is a downstream fork of the public Zephyr Project repository, and it includes device support for a wide range of Silicon Labs wireless SoCs. The result is a more cohesive development experience, especially for wireless IoT applications.The result is a more cohesive development experience, especially for wireless IoT applications.The result is a more cohesive development experience, especially for wireless IoT applications.

Simplicity SDK brings together peripheral drivers, wireless stacks, and device support in a way that reduces the friction typically associated with embedded development. For example, connectivity options such as Bluetooth LE, Thread, and Matter are aligned with the underlying hardware capabilities, allowing developers to focus more on application logic and less on integration challenges. The development flow is managed by West, Zephyr’s powerful meta tool, which offers ample opportunities for customization and expansion of new projects.

Silicon Labs devices with Secure Vault™ provide a number of best-in-class security capabilities that complement Zephyr’s software-based security features. Together, they create a layered approach that addresses both software and hardware attack surfaces with minimal effort needed from developers.


Simplicity SDK for Zephyr Reduces IoT Development Trade-offs

The true appeal of Simplicity SDK for Zephyr does not necessarily lie in any individual feature, but in the total solution’s ability to reduce the trade-offs IoT developers typically face. Instead of choosing between flexibility and integration, or between open ecosystems and production readiness, teams can work within a framework that supports all of the above.

In today’s development environment, selecting the right RTOS fundamentally depends on the priorities of the project. For simple, standalone devices, a lightweight solution may still be sufficient. For highly specialized applications, a proprietary system might offer short-term advantages. But for connected, secure, and scalable IoT products, the trend is clearly toward platforms that combine open standards with strong ecosystem support.


Select the Best RTOS for Embedded Systems

As the demands on embedded systems continue to grow, the decision is less about selecting a kernel and more about choosing a development foundation. In that context, solutions that emphasize security, flexibility, and streamlined development workflows are likely to shape the next generation of connected devices.

Learn more about Simplicity SDK for Zephyr.

CATEGORIES: IoT Insights
Sai Ananya Tungaturthi
Sai Ananya Tungaturthi
Associate Product Manager
Close
Loading Results