The Advantages of Low-Cost OpenThread Border Router (OTBRs) in Matter over Thread Integration

08/26/2025 | Devanjan Sikdar | 2 Min Read

In the rapidly evolving world of smart home technology, seamless integration and user-friendly experiences are paramount. One of the latest advancements in this field is the implementation of OpenThread Border Router (OTBR) functionality in devices, which bridges the gap between different network protocols like Matter over Thread and Wi-Fi. This innovative approach not only enhances the reliability of the smart home network but also offers a cost-effective solution for ensuring robust connectivity.


HRAPs Are Making OTBRs More Common in Today’s Smart Homes

Today, stand-alone smart devices like voice assistants or TVs are incorporating OTBR functionality, supporting both Matter over Wi-Fi and Matter over Thread. While these devices aren’t the central Wi-Fi hub in the home, they serve as critical bridges that connect Thread-based devices to the broader Matter ecosystem over Wi-Fi.

With the release of Matter 1.4, the Connectivity Standards Alliance (CSA) is paving the way for more OTBR devices with support for Matter-certified HRAP (home routers and access points). These devices are accelerating the shift toward a standardized approach in which smart home devices support both Matter over Wi-Fi and Matter over Thread out of the box. As a result, Matter over Thread is quickly becoming a core part of the connected home landscape.

Silicon Labs is helping enable this transformation with cost-effective solutions like the SiWx917, which makes it easier for device makers to build dual-protocol Matter products.


Improving Network Reliability with OTBR

The integration of OTBR functionality in devices significantly improves the reliability of the smart home network. In homes with multiple OTBRs, redundancy is also built in—if one device fails, another can seamlessly take over, ensuring a more resilient and reliable smart home experience.

Here’s how:


Eliminating Single Points of Failure

Low-cost OTBRs can be deployed to create multiple points of connectivity within the Matter fabric. By eliminating a single point of failure, OTBRs ensure that the network remains operational even if one device or connection fails. This redundancy enhances the overall reliability of the smart home setup.

In traditional smart home networks, a single device failure can disrupt the entire system. By deploying multiple OTBRs, manufacturers can create a mesh network that reroutes data through alternate paths, ensuring continuous operation and minimizing downtime. As the of implementation comes down with devices like the SiW917 and the MG21, this gets easier. For a closer look at how OTBR helps in this area, Silicon Labs' senior product marketing manager and resident smart home enthusiast, Matt Maupin, recently shared his first-hand experience testing Matter over Thread in this blog post.


Enhancing Interoperability

One of the key benefits of Matter and OTBR integration is the reduction of compatibility issues. This improvement enhances the user experience, reduces product returns, and fosters customer loyalty. Users can seamlessly add new devices to their smart home network without worrying about interoperability problems.

Matter's standardized protocols enable devices from different manufacturers to work together harmoniously. OTBR further strengthens this interoperability by bridging Thread and Wi-Fi networks, allowing users to integrate a diverse range of devices into their smart home ecosystem.


Cost-Effective Solutions

Low-cost OTBRs provide an affordable option for enhancing the reliability of the smart home network. By reducing the hardware requirements and simplifying the integration process, manufacturers can offer high-quality, reliable products at a lower cost. This accessibility opens up the smart home market to a broader audience, ensuring that more consumers can benefit from advanced smart home technologies.

Affordable OTBR solutions democratize smart home technology, making it accessible to a wider range of consumers. This inclusivity drives market growth and encourages innovation, as more users adopt and experiment with smart home devices.


Easy Implementation of OTBR Functionality is a Significant Step Forward

By improving network reliability and offering cost-effective solutions, OTBR bridges different network protocols, ensuring a unified and user-friendly smart home experience. As the smart home ecosystem continues to evolve, innovations like OTBR will play a crucial role in shaping the future of connected living.

The widespread adoption of OTBR in Matter-enabled devices signifies a new era of smart home connectivity. With enhanced reliability, security, and scalability, OTBR empowers users to create intelligent and responsive living environments, transforming everyday experiences.

Devanjan Sikdar
Devanjan Sikdar
Product Marketing Manager
Close
Loading Results