Designing for India’s Smart Meter SLAs: Why Wi-SUN Is the Foundation for Utility-Grade Performance

06/24/2026 | Chad Steider | 3 Min Read

The Government of India’s Revamped Distribution Sector Scheme (RDSS) is one of the most ambitious infrastructure upgrades in the world, with the goal of transitioning 250 million conventional meters to smart meters by 2027. Driven by grid modernization programs like RDSS and others, utilities are deploying intelligent networks at unprecedented scale, often spanning millions of endpoints.

The scale of the project is ambitious, but one of the most important challenges is meeting the strict service level agreements (SLAs) in environments where performance directly impacts revenue, reliability, and customer trust. Advanced Metering Infrastructure (AMI) is one of the key technologies being deployed through RDSS and it comes with high expectations for utility providers to meet the SLA requirements. For example, 99.9% of commands issued to smart meters must be completed successfully within defined response windows, typically no more than 15 minutes from initiation. Two performance metrics are particularly important: fast response times for real-time meter operations and rapid restoration of network connectivity after power interruptions.

These requirements fundamentally shift how networks must be designed. Connectivity is no longer enough. What matters is predictable, system-level performance at scale.


Why Traditional Network Approaches Fall Short for India Smart Meter SLAs

Many connectivity technologies can establish links across long distances. Far fewer can maintain consistent performance under the demands of large-scale utility networks.

Cellular introduces ongoing operational costs and limits control over network behavior. LPWAN technologies often struggle with downlink efficiency, making large-scale firmware updates difficult. Proprietary mesh networks may work in smaller deployments but can lack the scalability, interoperability, and predictability required for national infrastructure.

At India’s scale, maintaining performance across thousands of nodes operating simultaneously is critical.


The Metrics That Actually Define Smart Meter SLA Compliance

To meet SLA requirements, utilities have to look beyond radio specifications and evaluate how networks behave under real-world conditions, including:

  • Network formation and re-formation time
  • Latency across multi-hop paths
  • Throughput under load
  • Over-the-air (OTA) update efficiency

High PHY data rates do not guarantee real-world performance. Factors like routing overhead, channel access, multi-hop forwarding, and network congestion all influence end-to-end behavior. SLA compliance depends on how these elements work together rather than on any single specification.


Wi-SUN FAN 1.1 is Designed for Performance at Scale

Wi-SUN FAN 1.1 was built specifically to address these challenges. Its standards-based, IPv6 mesh architecture enables scalable, interoperable networks designed for utility-grade performance. More importantly, its performance has been validated under real-world conditions. Silicon Labs operates a Large Test Network (LTN) in our Rennes, France office, with more than 1,000 nodes, to provide insight into how Wi-SUN behaves at scale, including:

  • Self-healing recovery and high availability
    In large deployments, outages are inevitable. Wi-SUN networks demonstrate strong self-healing capabilities, with approximately 90% of nodes reconnecting rapidly after disruption. This supports availability targets of 99.5% and above.
  • Predictable latency across multi-hop networks
    Latency increases with hop count, but in a controlled and predictable way. Even in large networks, response times remain within the bounds required for command and control operations, typically within 5 to10 seconds.
  • Efficient OTA for large-scale deployments
    Firmware updates are often a bottleneck in large networks. Wi-SUN FAN 1.1 addresses this with broadcast OTA and higher throughput modes, significantly reducing update times and enabling completion within operational windows.
  • Scalability Proven in Real Deployments
    Validated performance at 1,000+ nodes per network segment demonstrates that Wi-SUN can scale without compromising reliability or responsiveness.

These characteristics are not theoretical and align directly with the SLA requirements defined for India’s AMI deployments.


From Specification to Smart Meter SLA Compliance

One of the key lessons from large-scale smart metering deployments is that SLA compliance cannot be achieved through isolated features. It requires a network designed holistically for reliability under disruption, stability under load, efficiency in maintenance operations like OTA, and scalability across dense deployments.

Wi-SUN FAN 1.1 addresses these requirements as a complete system, combining standards-based interoperability, optimized routing and network behavior, and proven performance under real-world conditions.

This makes it uniquely suited for environments like India, where performance is measured continuously and at scale.


Building a Future-Ready Grid Network in India

India’s current AMI rollout is just the foundation for broader grid modernization.

Future applications, including distributed energy resources (DER), electric vehicle infrastructure, and advanced grid automation, will demand even more from communication networks. Because of this, utilities need a solution that not only meets today’s SLAs but can evolve alongside future requirements.

Wi-SUN provides that foundation:

  • A standards-based ecosystem that supports multi-vendor interoperability
  • A scalable architecture capable of growing with network demands
  • A performance profile validated for large-scale, real-world deployments


Meeting India’s Smart Meter SLAs Requires Predictable Performance at Scale

Large-scale deployments like this require platforms that can deliver low latency, fast network formation, and efficient OTA updates across potentially thousands of devices. Wi-SUN FAN 1.1 provides the standards-based foundation needed to meet these requirements, while Silicon Labs extends those capabilities with the FG28 wireless SoC and a production-proven Wi-SUN software stack. Designed for both infrastructure and advanced edge devices, the FG28 combines high-performance Sub-GHz connectivity with optional Bluetooth Low Energy (LE) support, enabling long-range networking alongside simplified commissioning, maintenance, and local device access. Together, our hardware and software platform helps utilities accelerate deployment, improve network reliability, simplify lifecycle management, and achieve the scalability needed for next-generation grid and smart city applications. The result is a complete solution that enables organizations to build, operate, and expand large outdoor IoT networks with greater confidence, performance, and efficiency.

Chad Steider
Chad Steider
Senior Manager, Product Marketing
Close
Loading Results
Close