Silicon Labs: 20 Years Leading Sub-GHz wireless

Silicon Labs: 20+ Years Leading Sub-GHz Wireless

11/12/2026 | Chad Steider | 2 Min Read

Sub-GHz products serve demanding applications, from battery-powered water meters to security sensors and large utility networks. Their requirements vary, but the underlying challenge is consistent: build reliable wireless products that meet today’s needs and keep working throughout a long service life.

Silicon Labs has shipped more than one billion Sub-GHz devices since 2007, and leads the industry with a broad Sub-GHz portfolio backed by nearly two decades of experience. Our offerings span radio transceivers, network co-processors and wireless SoCs, supported by software, development tools and experience from real-world deployments.


A Sub-GHz Portfolio Built Around Different Design Needs

There is no single architecture that fits every Sub-GHz product. A team adding connectivity to an established design may want to retain its host processor and application software. Another may want to offload wireless networking, while a new design may benefit from integrating the radio, stack, and application on one device.

Silicon Labs supports each approach. Customers can choose the architecture that fits their design, preserve existing product investments or pursue greater integration when the application calls for it.

The same principle applies across the portfolio. A battery-powered sensor places different demands on a wireless device than an electric meter or a network infrastructure product. Power consumption, memory, throughput, and application processing all affect the choice. A broad portfolio gives designers room to balance those requirements around the product they are building.

Field Experience That Matters Over the Life of a Product

Sub-GHz devices often remain deployed for a decade or more. For customers, reliable connectivity and efficient power consumption have consequences throughout that period: battery replacement, maintenance visits, service continuity, and the cost of supporting an installed fleet.

Silicon Labs brings nearly two decades of Sub-GHz experience across utility metering, wireless security, access control, and other demanding applications. That experience spans different RF environments, regional requirements, and wireless protocols.

Lab testing matters, but results in a lab can’t account for all real-world conditions. Equally important is experience with the conditions customers encounter in the field. For teams choosing a wireless platform, the track record of an established player in sub-GHz is a meaningful advantage.

Reliability for the Life of Your Product


Software is Central to the Sub-GHz Solution

The radio is just one part of bringing a connected product to market. Developers also need software that supports their chosen protocol and gives them access to the radio capabilities their application requires.

Silicon Labs’ Sub-GHz software offering includes Wi-SUN FAN 1.0 and FAN 1.1, alongside technologies such as Wireless M-Bus, mioty, and Zigbee Smart Energy. Field deployments and extensive network testing support the development of these solutions, including testing Wi-SUN performance at network scale.

For proprietary applications, Silicon Labs’ Radio Abstraction Interface Layer, or RAIL, provides a consistent interface to low-level radio features. It gives developers a foundation for implementing their own protocols while using Silicon Labs’ radio capabilities.

That combination of standards-based stacks and proprietary development support gives customers options across markets and product requirements. Software is a core part of what sets the portfolio apart.


Expanding with Application Requirements

Sub-GHz application requirements continue to grow. Some products need higher data rates to carry more information. Others need more memory as they adopt standards-based networking and accommodate larger software stacks and application code. More capable applications also call for additional processing within the wireless device.

Silicon Labs continues to expand its Sub-GHz portfolio to meet those needs, with investment in higher-throughput connectivity, greater memory capacity, and more application processing, while preserving the low-power performance that remains essential to long-life devices. Customers get more options as their products evolve, backed by the software and wireless experience needed to put those capabilities to work.


A Complete Foundation for Sub-GHz Development

Portfolio breadth matters when it helps customers solve the full design problem: selecting the right architecture, meeting power and performance requirements, implementing the wireless software, and supporting a product through years of operation.

Silicon Labs brings those capabilities together across a broad wireless portfolio, giving customers more choice today and a path to address new requirements as they emerge. That is the advantage of working with a Sub-GHz leader: deep design options, established software, and experience from real deployments.

Explore Silicon Labs’ Sub-GHz portfolio or request a meeting with Silicon Labs at CES 2027 January 6–9 in Las Vegas, and let’s explore what we can build together.

A Broad Portfolio to Fit Your Design Needs
Chad Steider
Chad Steider
Senior Manager, Product Marketing
Close
Loading Results
Close