2 Are PTP Unicast packets visible to Wireshark through a switch?
3 Are there any important parameters that should be taken into account when choosing a network switch chip to connect to the M88?
4 Can the module be synchronized to an input 1PPS without having a ToD input from the GPS?
5 Difference Between Engine Asymmetry and Port Asymmetry settings?
6 Do the modules support IGMP?
7 Does the AccuTime module have an SNTP server available?
8 Energy Efficient Ethernet
9 Ethernet LED meaning
10 How can 1PPS be enabled for syntonization from GPS when ToD is not available?
11 How can files be transferred to/from a AccuTime module file system from a host PC/laptop?
12 How can I tell that the slave is Synchronized to the master?
13 How can Clock Class during Holdover be set by CLI Commands?
14 How do I get firmware updates?
15 How do AccuTime modules communicate with external PHY?
16 How is checksum handled for IPv4 and IPv6?
17 How many clients does your master support?
18 How many other slaves can your slave handle?
19 How much does the modules weigh?
20 How much time does it take to synchronize?
21 How to interpret the sync status
22 How to transfer files using kermit on a Linux machine
23 Is a '00' Master Clock ID valid for an AccuTime module slave to sync to?
24 Is defining a fixed PPSOUT/FREQOUT relationship that is the same every time the M64 is restarted possible?
25 M88 CLK_REF specification
26 Running PTP over Ethernet (layer 2) on enet1
27 Setting DSCP for PTP
28 The two interfaces of M64 and M68
29 There is a 3 µs offset between master and slave's 1PPS. What do I do?
30 There is a leap second announced. What do I do?
31 What are some guidelines for the "ptp2 config" parameters for servo control?
32 What are the set up conditions required to get TOD outputs to activate on the module?
33 What are the Synchronization Requirements for Different Types of LTE?
34 What does the console output data represent when the module is run in Mode 4 (Debug)?
35 What is a guideline for setting the GPS Antenna cable delay value?
36 What is the command procedure to upload an module file to a PC using Kermit?
37 What is the difference between congruent and non-congruent mode when operating the M88 module?
38 What is the Ether type for Layer 2 and Layer 3 communication protocol?
39 What is the maximum overlap/delay that is acceptable for a AccuTime timing module between the TOD and the 1PPS input?
40 What is the module ToD interface and format?
41 What is the normal boot process for the modules?
42 What is the recommended power sequencing for M88?
43 What is the Re-flow profile required for M6x module?
44 What NMEA messages are used for TOD input and output?
45 What PTP switches can be used with the AccuTime module IEEE 1588-2008 equipment?
46 What the preferred PTP Engine Mode for a module Clock with multiple PTP ports and configured as a Boundary Clock or Gateway Clock when the Primary Timing Source is GPS?
47 What time scale is used by PTP and what is the relationship to other time scales?
48 What's the difference between a one-step master and a two-step master?
49 What's the maximum operating temperature for M64/M68?
50 What's the MTBF for M88
51 Why are there 4 bytes after the PTP message?
52 What happened to support for the M50 and the development kit.
Timing Knowledge Base
M64/M68/M88 Modules for IEEE 1588 FAQs
See attached PDF for articles:
1 Adjusting the PPS out
2 Are PTP Unicast packets visible to Wireshark through a switch?
3 Are there any important parameters that should be taken into account when choosing a network switch chip to connect to the M88?
4 Can the module be synchronized to an input 1PPS without having a ToD input from the GPS?
5 Difference Between Engine Asymmetry and Port Asymmetry settings?
6 Do the modules support IGMP?
7 Does the AccuTime module have an SNTP server available?
8 Energy Efficient Ethernet
9 Ethernet LED meaning
10 How can 1PPS be enabled for syntonization from GPS when ToD is not available?
11 How can files be transferred to/from a AccuTime module file system from a host PC/laptop?
12 How can I tell that the slave is Synchronized to the master?
13 How can Clock Class during Holdover be set by CLI Commands?
14 How do I get firmware updates?
15 How do AccuTime modules communicate with external PHY?
16 How is checksum handled for IPv4 and IPv6?
17 How many clients does your master support?
18 How many other slaves can your slave handle?
19 How much does the modules weigh?
20 How much time does it take to synchronize?
21 How to interpret the sync status
22 How to transfer files using kermit on a Linux machine
23 Is a '00' Master Clock ID valid for an AccuTime module slave to sync to?
24 Is defining a fixed PPSOUT/FREQOUT relationship that is the same every time the M64 is restarted possible?
25 M88 CLK_REF specification
26 Running PTP over Ethernet (layer 2) on enet1
27 Setting DSCP for PTP
28 The two interfaces of M64 and M68
29 There is a 3 µs offset between master and slave's 1PPS. What do I do?
30 There is a leap second announced. What do I do?
31 What are some guidelines for the "ptp2 config" parameters for servo control?
32 What are the set up conditions required to get TOD outputs to activate on the module?
33 What are the Synchronization Requirements for Different Types of LTE?
34 What does the console output data represent when the module is run in Mode 4 (Debug)?
35 What is a guideline for setting the GPS Antenna cable delay value?
36 What is the command procedure to upload an module file to a PC using Kermit?
37 What is the difference between congruent and non-congruent mode when operating the M88 module?
38 What is the Ether type for Layer 2 and Layer 3 communication protocol?
39 What is the maximum overlap/delay that is acceptable for a AccuTime timing module between the TOD and the 1PPS input?
40 What is the module ToD interface and format?
41 What is the normal boot process for the modules?
42 What is the recommended power sequencing for M88?
43 What is the Re-flow profile required for M6x module?
44 What NMEA messages are used for TOD input and output?
45 What PTP switches can be used with the AccuTime module IEEE 1588-2008 equipment?
46 What the preferred PTP Engine Mode for a module Clock with multiple PTP ports and configured as a Boundary Clock or Gateway Clock when the Primary Timing Source is GPS?
47 What time scale is used by PTP and what is the relationship to other time scales?
48 What's the difference between a one-step master and a two-step master?
49 What's the maximum operating temperature for M64/M68?
50 What's the MTBF for M88
51 Why are there 4 bytes after the PTP message?
52 What happened to support for the M50 and the development kit.
53 Revision History