Bluetooth NCP Commander
The Simplicity Bluetooth NCP Commander is a tool for sending BGAPI commands to NCP target applications. It offers an intuitive GUI for controlling BLE or Bluetooth Mesh NCP targets, allowing users to learn the Bluetooth API, launch commands via a smart console, perform common BLE functions, manipulate GATT databases, and provision Bluetooth Mesh devices.
- Overview
Overview
Key Features
Control the NCP target intuitively through a graphical user interface and learn the inner workings of the Bluetooth API
Launch commands effortlessly through the smart console with built-in documentation and intellisense
Perform the most common BLE functions (advertising, scanning, connections)
Manipulate the GATT database on the NCP target leveraging Dynamic GATT feature on the embedded stack
Provision and configure Bluetooth Mesh devices
- Getting Started
Getting Started
Step 1: Download and Install Simplicity Studio
Select your operating system (Windows/macOS/Linux) and follow the installation instructions. Complete the installation using the provided setup instructions.
A. Choose Full Installation (Recommended)
When prompted during installation, select the Full Install option.
Note: Choosing Full Install is the easiest way to make sure you have all tools available right away.
B. Manual Installation via Package Manager (Optional)
If you skip Full Install, you can install individual tools as needed:
- Open Simplicity Studio
- Go to Package Manager
- Browse or search for the desired tool under the Tools tab
- Select and install it
Note: This method is useful if you prefer a minimal setup or only need specific tools.
Step 2: Launching and Using a Tool
- Launch Simplicity Studio
- Go to the Tools menu on the left side
- Select the installed tool and click to the “Play” or the “Open Tool” button
- If the tool doesn’t appear, confirm it is installed via the Package Manager
Tool Dependencies - Some tools may require support packages
- Tech Docs
Tech Docs
Documentation
Access the latest guides and technical documentation below. Look for documentation specific to your tool.
- Community & Support
Community & Support
Join the Community & Get Support
Post questions or browse discussions on the Silicon Labs Community. Check out developer blogs, application notes, and training videos.