2026 Tech Talks
Built by developers for developers, Tech Talks deliver practical training, expert guidance, and technical insights to help you build with confidence.
Register for upcoming Tech Talks below and explore our library of on-demand Tech Talks to catch up on past sessions.
From Evaluation to Production: Using Open Source and Communities to Accelerate IoT Development, Featuring Arduino
October 22
IoT development increasingly happens within an open ecosystem spanning open-source software, GitHub repositories, development platforms, and communities where developers exchange knowledge, solve problems, and contribute new ideas. Together, these resources make it easier for developers to discover technologies, accelerate evaluation and integration, and draw on shared expertise throughout the development process.
In this Tech Talk, we’ll explore how Silicon Labs is expanding the developer experience through open-source software and participation in developer communities. We’ll look at how open development provides greater visibility, collaboration, and access to resources while complementing the tools, software, testing, and support needed to develop production-ready IoT products.
We’ll then put this into practice through Arduino. Using Silicon Labs-powered Arduino boards and community resources, we’ll show how developers can get started with wireless IoT development and explore Matter over Thread, Zigbee, and Bluetooth LE within the familiar Arduino ecosystem, together with available OpenThread RCP and Zigbee NCP resources. We’ll walk through available hardware, software, examples, and community support and demonstrate how these resources help developers move from exploration to working applications.
Finally, we’ll show how the same Silicon Labs-based hardware can provide a path beyond initial prototyping. Developers can begin with familiar Arduino APIs and later move to native Zephyr or Silicon Labs’ professional development workflows as their requirements grow—without necessarily changing the underlying hardware platform.
Register Now
Navigating the EU Cyber Resilience Act: What It Means for Connected Products
November 19
This session will provide an accessible introduction to the Cyber Resilience Act (CRA) and its potential relevance for organizations developing, delivering, or managing digital products. We’ll explore the broader intent behind the regulation, the themes it brings into focus, and the practical questions teams may wish to consider as the landscape evolves.
The session will also include Silicon Labs’ perspective on CRA and how we are thinking about its relevance to our products and customers.
Designed as a high-level discussion, the talk will create space for shared learning and future conversation without presuming a one-size-fits-all approach.
Register Now
Watch On-Demand Tech Talks
Amazon Sidewalk in 2026: Platform Evolution, New Use Cases, and What Comes Next
February 3
Join Silicon Labs and Jay Desai, General Manager, Amazon Sidewalk, for a focused discussion on the continued evolution of Amazon Sidewalk and the opportunities emerging in 2026. We will cover Amazon's recent platform updates including location services, future plans, and the expanding set of use cases and device types Amazon Sidewalk is enabling across the smart home, smart city, and industrial IoT markets.
Silicon Labs will outline our complete Amazon Sidewalk solution including hardware, software, security, and development tools, and demonstrate how these resources help device makers accelerate design, simplify certification, and deliver reliable, low-power products to market.
This session is ideal for teams exploring Amazon Sidewalk or preparing to scale deployments.
Watch On-Demand
Simplicity SDK for Zephyr
February 19
This session provides an introductory look at Silicon Labs’ Simplicity SDK for Zephyr and explores why we are embracing Zephyr and the broader OpenSource ecosystem. We will outline the goals of the SDK, highlight the benefits of a unified development framework, and discuss how an OpenSource approach can improve flexibility, collaboration, and long-term scalability for embedded applications.
Watch On-Demand
RF Performance in IoT End Devices - Is Good Enough Really Good Enough?
March 3
For IoT product developers, there are always tradeoffs to make between features, performance and cost. We often hear that RF performance just needs to be "good enough". But what does that really mean? RF performance will directly relate to the user experience and poor performance will affect areas like range, reliability, latency and even battery life. Some of these issues could result in a user blaming the end product, for example, limited range and poor battery life. Others like latency and reliability could be blamed on the end product, ecosystem or even the internet connection. However, all of these will hamper adoption, which is a losing proposition for everyone involved.
This session will look at how a chipset's specifications and features including link budget, blocking, rejection and antenna diversity can drastically affect the RF performance of IoT end devices. At the end of this session, you should be able to understand these areas better to guide you on what RF performance is really good enough for your IoT products.
Watch On-Demand
Matter Energy Management
March 19
As smart home platforms converge around Matter, energy management is emerging as a major opportunity for the next wave of connected experiences. This webinar will explore how interoperable devices can help unlock smarter energy insights and automation in the home—improving comfort, cost control, and grid friendliness. We’ll provide insight to the markets while discussing what's possible today, what’s coming next, and how different stakeholders can use these capabilities to deliver real value across products and programs.
Watch On-Demand
The Untapped Potential of Wireless SoCs: From Connectivity to System Consolidation
April 7
Wireless SoCs are still often treated as radios, paired with external MCUs for control and intelligence. But modern devices have significant compute headroom that frequently goes unused. This talk explores how wireless connectivity, real-time control, and even edge AI can coexist on a single device without compromising performance. As IoT systems evolve, the opportunity is clear: rethink system partitioning and design around the compute already inside your wireless SoC.
Watch On-Demand
Hands-On Edge AI: Developing Embedded AI/ML Applications
April 23
AI/ML at the edge is rapidly transforming how IoT devices sense, interpret, and respond to the world around them. But moving from concept to a working embedded AI application can feel complex and fragmented.
This Tech Talk is designed to simplify that journey.
In this session, we will build an AI/ML application step-by-step, walking through the full development flow from model integration to deployment on an embedded device. The focus will be on practical implementation — understanding how models move from development to embedded inference, how performance and memory tradeoffs are evaluated, and how tooling supports efficient iteration.
By the end of the session, you’ll have a clearer roadmap for bringing AI/ML capabilities into your own embedded designs.
Watch On-Demand
Connected, Responsive, and Efficient: Getting the Most Out of Your Low-Power Wi-Fi Devices
May 5
Wi-Fi IoT devices have had advantages over other low power wireless technologies at the edge through its higher bandwidth and large install base. Now we are seeing Wi-Fi pushing into roles once reserved for lower power, battery operated wireless technologies as well. The purpose for Wi-Fi is no longer just connectivity, but achieving useful battery life while remaining securely associated, responsive, and scalable in dense networks. Modern Wi-Fi power-saving features are specifically aimed at reducing radio wake time, extending sleep intervals, and lowering unnecessary exchanges with the access point. These features enable longer sleep periods and less frequent infrastructure communication for low-power devices. Wi-Fi 6 brought major efficiency tools such as Target Wake Time (TWT), while Wi-Fi 6E extends those same Wi-Fi 6 capabilities into 6 GHz. Wi-Fi 7 builds on this foundation with further improvements in efficiency, latency, and operation across a wider variety of device classes and channel configurations.
Attendees will leave with a practical understanding of how modern Wi-Fi features can be used to design battery-powered edge devices that stay connected longer without sacrificing responsiveness or security. They will also gain a clearer view of where Wi-Fi 6, 6E, and 7 fit in low-power IoT strategies, helping them evaluate when Wi-Fi is the right choice versus other low-power wireless options.
Watch On-Demand
Expanding LPWAN Deployment Models: Enabling Both Large-Scale and Segmented Micro-Mesh Networks
May 21
LPWAN technologies have enabled some of the world’s largest and most reliable outdoor IoT networks, particularly in utility and smart city deployments. As the market expands into commercial, industrial, and campus-scale applications, a complementary deployment model is emerging alongside these large-scale networks.
This session explores how segmented, site-level “micro-mesh” networks are enabling a new class of deployments that prioritize faster rollout, lower infrastructure cost, and simplified operations. We will examine how architectures are evolving, including the role of simplified, SoC-based border routers and flexible backhaul options such as Wi-Fi and LTE.
Attendees will gain a practical understanding of how technologies like Wi-SUN, along with other LPWAN approaches such as Mioty and Wirepas, map to different deployment models. The session will provide guidance on how to select the right architecture based on scale, topology, and operational requirements, and how to design networks that balance performance, cost, and long-term manageability.
Watch On-Demand
Bluetooth Channel Sounding: From Performance to Real-World Applications
June 2
As IoT devices become more context-aware, spatial awareness is emerging as a key capability for enabling more secure, responsive, and intuitive user experiences. Bluetooth Channel Sounding is a practical new approach to delivering that awareness, combining improved ranging accuracy with the scalability and ecosystem reach of Bluetooth. In this Tech Talk, Silicon Labs will provide a practical look at Channel Sounding through a brief technology overview, Silicon Labs algorithm approaches and their performance trade-offs, and the software support available to accelerate development.
Attendees will also get a sneak peek at upcoming Silicon Labs hardware for Channel Sounding and a look at what’s ahead.
Watch On-Demand
What’s Next for Bluetooth LE with Bluetooth SIG
June 18
Bluetooth is evolving beyond traditional connectivity into a platform that enables spatial awareness, secure proximity detection, and high‑performance, context‑aware systems. This evolution is driven by a rapidly advancing Bluetooth ecosystem powered by a global community of developers, engineers, and industry leaders.
In this Tech Talk, we will explore how Silicon Labs, together with the Bluetooth SIG, are shaping the future of secure, precise, and interoperable Bluetooth technologies. The session provides a technical overview of three key innovations defining the next phase of Bluetooth.
We begin with Bluetooth® Channel Sounding, examining recent advancements in secure distance measurement and ranging accuracy, along with emerging applications and security enhancements that enable reliable proximity awareness in real‑world deployments. The discussion then turns to Ultra‑Low Latency HID (ULL HID), highlighting how Bluetooth is optimized for highly responsive human interface devices through reduced latency and improved performance for interactive use cases. Finally, we explore High Data Throughput (HDT) and how it expands Bluetooth capabilities for data‑intensive applications, enabling higher throughput while maintaining efficiency and interoperability.
Join Silicon Labs and the Bluetooth SIG for a comprehensive technical view of Bluetooth innovation and how these features fit into the broader Bluetooth roadmap.
Watch On-Demand
Extending Bluetooth LE Tracking via Satellite, Featuring Hubble Network
September 1
What if your Bluetooth® LE devices could transmit from almost anywhere on Earth, well beyond the reach of traditional wireless networks? Sensor readings, status, telemetry, whatever data you can't afford to lose.
Long range connectivity has traditionally required specialized hardware and increased power consumption. Hubble Network takes a different path: standard Bluetooth LE silicon, heard directly by satellites and by a global network of 100M million terrestrial gateways, with no hardware changes at all.
Join Silicon Labs and Hubble Network to see the technology behind Hubble's satellite-enabled IoT solution, and how it extends Bluetooth LE range from meters to hundreds of kilometers using the Silicon Labs EFR32MG24 wireless SoC.
You'll see real-world satellite and terrestrial connectivity in action, how quickly you can provision and monitor devices on the Hubble platform, and how to integrate Hubble's SDK into your existing Bluetooth LE designs. We'll also walk through the hardware, software, documentation, and development resources available to get your first Hubble-enabled device to market.
Watch On-Demand
Navigating Matter Certification: What’s Changed and How to Succeed
September 17
Matter certification has evolved significantly since the release of Matter 1.0, with the Connectivity Standards Alliance (CSA) streamlining certification requirements, improving testing processes, and reducing the effort required to bring certified products to market. This Tech Talk focuses on the certification journey—from understanding the current Matter certification requirements to navigating the latest CSA processes and tools. We'll review what's changed over the past three years, discuss the latest Matter specification updates impacting certification, and demonstrate how Silicon Labs simplifies development, pre-certification testing, and compliance validation to help reduce risk, accelerate testing, and achieve Matter certification with confidence.
Watch On-Demand
Wireless SoC Evolution: Balancing Compute, Power, Cost, and Complexity
October 6
Wireless IoT applications are evolving rapidly. Devices that once only sensed, slept, and transmitted small packets are now expected to support Matter, multiprotocol connectivity, stronger security, over-the-air (OTA) updates, richer user experiences, and even AI at the edge. At the same time, customers continue to expect long battery life, low cost, robust wireless performance, long product lifetimes, and shorter development cycles.
As these requirements evolve, wireless SoC architectures must evolve as well. This talk examines the key architectural considerations behind modern wireless platforms, including compute, memory, connectivity, security, power management, system integration, and the engineering tradeoffs involved in balancing performance, energy efficiency, software complexity, RF design, and cost.
Through both customer and developer perspectives, attendees will gain a practical framework for evaluating wireless platforms, understanding how architectural decisions impact real-world product requirements, and selecting the right platform for the right application.