Deilvering Secure NFC Tap-to-Unlock with Aliro

Silicon Labs Delivers Bank-Grade Cryptography for NFC Tap-to-Unlock With Ultra-Low-Power 15.4

02/25/2026 | Scott Farester | 3 Min Read

With the release of Aliro 1.0, the Connectivity Standards Alliance (CSA) has taken another step in its mission to unify the smart home, this time by expanding access control across smart locks and ecosystems. Aliro is a standardized credential and communication protocol that enables devices to make access decisions, bringing true tap-to-unlock functionality to consumers. Now, instead of pulling out your phone, opening an app, waiting for it to load, and finding the unlock button, tap-to-unlock works instantly. The experience becomes faster and hassle-free, similar to using a contactless payment card. It also helps device makers accelerate development with a proven, ready-to-build platform designed for secure credentials, flexible connectivity options, and low-power performance.

Durin, Inc. is one of the first device makers to support the new application layer with the recent launch of its Durin Door Manager. The next-generation device works with existing smart locks and features the Silicon Labs MG24 wireless SoC. With the MG24, Durin can validate credentials and protect keys on a single secure wireless platform while the integrated cryptography accelerator keeps performance fast for end users.


Aliro: One Standard for Digital Keys Across Wallets

Beyond making the smart lock user experience smoother, Aliro provides a standardized way to access digital smart wallets across brands. Previously, implementing this required separate processes for Google Wallet, Samsung Wallet, and Apple’s HomeKit/HomeKey, often resulting in added complexity and fees. With Aliro, ecosystem providers can simplify the experience for home users by letting digital keys live directly in the phone’s digital wallet. Users just tap their phones to the reader, with no need to open a separate app or go through multiple steps.


Silicon Labs Accelerates NFC Tap-to-Unlock Access with Integrated Crypto and Wireless Performance

Silicon Labs is helping simplify development by integrating NFC directly into its SDK for Aliro-enabled solutions. This includes a tested and validated NFC transceiver driver, along with hardware-accelerated encryption and secure key management on all Silicon Labs Matter-enabled devices, giving developers confidence and reducing integration effort.

All tap-to-unlock and supporting features, including support for step-up authentication requirements, are included in Silicon Labs’ standard SDK release, making it possible to perform key validation and Access Document verification in a single NFC transaction. Because tap-to-unlock is a core requirement for Aliro certification, this integrated approach gives manufacturers a streamlined, secure path to compliance and a faster time-to-market.

Tap-to-unlock is the baseline requirement for Aliro certification, but our multiprotocol platform also enables true hands-free access, as with the Durin Door Manager.


Aliro is Unlocking New Areas in Access Control

Matter is foundational to hands-free access for commissioning devices, enabling advanced features like digital keys that allow access during specific windows of time. It also makes it so that homeowners don’t have to use different apps from various lock manufacturers. Until now, access control has been fragmented, requiring specific apps supplied by lock manufacturers. To unlock the front door, users are required to open the app that corresponds to the lock. Even in cases where tap-to-unlock is available, launching an app is necessary to gain access. When locks are tied to a single ecosystem, it limits the benefits for users. With Aliro, homeowners can change platforms or ecosystem providers without replacing their lock. And households that include Android users and Apple users can share the same seamless experience. That cross-ecosystem consistency and long-term flexibility are key.

Before Aliro, developers were required to engage every ecosystem provider individually, which included building separate firmware and software integrations as well as paying for access. Now, one implementation can work broadly across devices. This reduces costs for R&D and certification, and cuts time to market.


Bank-Grade Cryptography for Tap-to-Unlock

With Aliro, the security model is very similar to what people already trust for tap-to-pay. When you tap your phone to a lock, you’re using the same class of bank-grade cryptography that includes public and private keys securely stored on the device. As the NFC interaction happens, Aliro runs a rapid sequence of cryptographic checks, which consists of multiple key exchanges happening in just milliseconds. This includes five separate transactions, including verifying the credentials and proving that the device and the lock both hold the correct key pair. Only after that verification does access get granted. Being able to perform these calculations fast is required for a true tap-to-unlock experience. Silicon Labs’ Matter-enabled devices can execute Aliro’s cryptographic exchanges in milliseconds, combining optimized hardware security, low-latency NFC, and efficient wireless stacks to make tap-to-unlock feel instant.


Why Silicon Labs’ Matter Hardware and Aliro Standard Win

Silicon Labs and Aliro are a good pairing because of our leadership position in advancing Matter and purpose-built hardware that accelerates encryption and decryption. This combination enables secure, low-latency authentication and access control without sacrificing power efficiency or user experience. In a market long defined by fragmented, proprietary approaches to mobile credentials and reader communication, Aliro is important. By establishing a common, secure foundation for how user devices and access points interact, the new Aliro standard reduces complexity, increases interoperability, and enables trusted access experiences that scale cleanly across ecosystems, form factors, and deployment models.

Scott Farester
Scott Farester
Staff Product Marketing Manager
Close
Loading Results
Close