SLWSTK-COEXBP

MSRP $149.00

Wi-Fi Coexistence Evaluation Kit

The SLWSTK-COEXBP has reached Not Recommended for New Design (NRND) status due to the included devices being NRND.

The Wi-Fi Coexistence Development Kit provides a simple, but flexible evaluation board for developing managed coexistence between Wi-Fi, Zigbee, Thread, and Bluetooth radios. Managed coexistence is critical when putting multiple 2.4 GHz radios in today’s small hubs and gateways. With Silicon Labs coexistence backplane, developers can connect Wi-Fi and up to 3 Silicon Labs radios using a flexible PTA (Packet Traffic Arbitration) implementation to help manage radio operation. The backplane provides connections between the Wi-Fi system and the Silicon Labs Zigbee, Thread, and Bluetooth radio boards. 

MSRP $149.00

 
  • Enables prototyping of a managed coexistence solution
  • Supports Silicon Labs Zigbee, Thread, and Bluetooth devices
  • Supports Wi-Fi and up to 3 additional WSKT radio boards
  • Supports 1, 2, and 3 wire PTA signaling
  • Provides header for observation of PTA signals on logic analyzer
  • Supports both SoC and NCP software architectures

Step 1: Get Started with the User Guide

Step 2: Configure the Wi-Fi Coexistence and Perform Testing

  • Using a PTA capable Wi-Fi solution, configure the PTA interface on the EFR32 based Bluetooth, Zigbee, or Thread solution along with the PTA interface of your Wi-Fi device using the instructions and guidance found in UG103.17, UG350, AN1017 and AN1128.
  • Use the SLWSTK-COEXBP kit to test and evaluate the PTA performance of your solution which should include throughput scenarios for your application.
Note: Not all Wi-Fi solutions are capable of supporting PTA. When choosing a Wi-Fi solution, be sure to select a vendor and a Wi-F solution that supports coexistence/PTA operation.

Knowledge Base Articles

Browse our knowledge base articles for information about specific products.

User Forums

Browse technical questions, share your ideas, and learn more about our latest solutions.

Questions? You're in the Right Place.

Silicon Labs has an active, knowledgeable user community of engineers and developers that are enthusiastic about solving problems.

Close
Loading Results
Close