Protocol Life Cycle

Silicon Labs will add new features based on market requirements and continously improve the Z-Wave Protocol to position the Z-Wave Ecosystem. The Z-Wave Protocol Life Cycle is a process to provide rapid innovation, new features and robust matured protocol release to Z-Wave Partners. The Z-Wave Protocol Life Cycle defines the maturation process of Z-Wave Protocol generations and consist of three phases divided in five Life Cycle stages.

Please refer to the latest release notes for the life cycle status

protocol-life-cycle.jpg

Ascent Phase (BETA)

Silicon Labs releases new Z-Wave protocol generations (branches), i.e. initial BETA release of a Z-Wave Protocol generation that will introduce major new features/functions or support for a new Z-Wave Single Chip generation.

Maturity Phase (ACTIVE/MAINTAINED)

Each new generation will generate follow on matured releases to resolve protocol issues prioritized by Silicon Labs and based on input from Z-Wave Alliance Partners.

Decline Phase (MONITORED/OBSOLETE)

After a period of 17-24 months in the maturity phase a branch/release is discontinued and for an additional period (up to 24 months) a discontinued branch/release will be monitored since products based on this branch may still be shipping or under warranty in the field.

Life Cycle Status
(Phase)
Version Number (Example)Overview/Recommend UseSupport ProvidedNew FeaturesMinor Change Request AddedSevere Issues FixedModerate
/Minor Issues Fixed
Presence of Issue Verified
BETA
(Ascent Phase)
X.50Relase to provide early access to new features and enabling early development & testing.
Not for volume production - BETA release will immediately enter OBSOLETE status once a matured release is active for the same branch.
- BETA version will not be released with known servere issues, but may have moderate or minor issues
- Protocol issues found on in BETA release are fixed in forthcoming release
YESYESN/AN/AN/A
ACTIVE
(Maturity Phase)
X.27

X.28, X.29 ... X.2n

Matured release for volume production

Subsequent ACTIVE releases introduced as bug-fix releases or additional minor functionality. Recommended for volume production

- Full support on ACTIVE releases based on classification of issues
- New matured releases are provided typically 5-8 every months 
——YESYESYES 
MAINTAINED
(Maturity Phase)
X.25Status of the previous version, once a new version of the same branch is released. Not recommended for new products- Support is provided
- Protocol issues is provided through Z-Wave Technical Service (ZTS) website
- Protocol issues are fixed in the corresponding ACTIVE release
——YES—YES
MONITORED
(Decline Phase)
X.06Status when branch/release is three or more generations older than newest ACTIVE branch/release. OEM is recommended in upgrading product(s) to newer branch release- Protocol issues reported or found will be verified on MONITORED releases
- Information is provided through ZTS website
———*—YES
OBSOLETE
(Decline Phase)
(X-1).2xMONITORED release will be OBSOLETE after a period up to 24 months.- No longer supported—————
Close
Loading Results
Close