Video Material

WFI-114: Dev Lab - SiWG917 Sleeping Wi-Fi HTTP Server

This material is 4 of 4 in the Wi-Fi 110: Develop with Wi-Fi.

This series of videos shows how to develop Wi-Fi applications using the SiWx91x family.

Overview

This follow-on Dev Lab shows how to apply sleep modes to the HTTP Server created in the previous Wi-Fi Dev Lab. Both the Network and Application processors in the Silicon Labs energy-efficient SiWG917 Wi-Fi 6 SoC are placed into sleep modes when the FreeRTOS system is idle. The APIs to enable this are covered in the video and their effects on the sleep current is shown in the Simplicity Studio v5 Energy Profiler.

Hardware:

Software:

Additional Resources:

        Hardware Required:

        Silicon Labs SiWx91x Pro/Dev/Explorer Kits

        Ezurio SI917Y Veda Explorer Kit

        Close
        Loading Results
        Close