WEBINAR

SE103: Getting Started with the Arduino Nano Matter

Get started developing Matter-over-Thread applications in the Arduino IDE for the Arduino Nano Matter board and review example applications. Watch on-demand.

About this Session

Get a head start developing Matter-over-Thread applications in the Arduino IDE for the Arduino Nano Matter board, featuring the Silicon Labs EFR32MG24 multi-protocol wireless SoC. This session will walk you through:

  • How Arduino and Matter make IoT device development available to all
  • Configuring the Arduino IDE to work with Silicon Labs-powered boards
  • Example applications available in the IDE 
  • Creating, compiling, flashing, commissioning, and using your first application
  • The structure and APIs used to create Arduino Matter applications
  • Enhancing example applications to work with externally connected peripherals
  • Using the EFR32MG24’s AI/ML Hardware Accelerator
  • Next steps and additional resources

Speakers

Martin Looker

Martin Looker
Application Training Manager
Silicon Labs

Duration

45 Minutes

Language Choice:

This video supports multiple languages using AI-powered translations. Select your preferred language from the dropdown,
then use the gear icon in the settings menu to adjust audio and subtitles.



Questions? You're in the Right Place.

Silicon Labs has an active, knowledgeable user community of engineers and developers that are enthusiastic about solving problems.

Close
Loading Results