Video Material

MAT-121: Dev Lab - Build a Matter Fan with the Arduino Nano Matter

This material is 11 of 11 in the Matter 110: Matter Developer Journey.

Learn about developing Matter devices using Silicon Lab's secure, intelligent, connected microcontrollers

Overview

In this Dev Lab, we expand the Arduino Matter Fan example from the Arduino IDE to control real hardware. Starting from the built-in Matter Fan framework, the project adds code to drive a 120mm PWM fan, monitor its RPM, animate addressable RGB LEDs, and display information on an OLED screen. The fan can be controlled through an app, a voice assistant, or the on-board button.

You’ll learn how to use the Matter APIs provided in the Arduino Core for Silicon Labs boards, integrate external libraries for displays and QR codes, and build hardware support for a fully functional connected device. The video also covers commissioning the fan into a Matter network, controlling it with Alexa, and viewing the device status directly on the OLED.

What you will learn:

  • How to expand the Arduino Matter Fan example to control physical hardware
  • How to connect and control a PWM fan, LEDs, and an OLED display
  • How to use the Matter APIs and data model in the Arduino IDE
  • How to commission a Matter device and control it through an app or voice assistant
  • How to use Arduino libraries to extend functionality and speed up development

Build a complete connected device that combines Matter connectivity with real hardware control using the Arduino Nano Matter and Silicon Labs Arduino Core.

Software Links:

Hardware Links:

Additional Links:

    Dev Lab - Build a Matter Fan with the Arduino Nano Matter

    Prerequisites:

    Arduino Nano Matter or other compatible board

    For additional hardware see Hardware Links in main description

    Close
    Loading Results