Series 2 Brings Consolidation, Simplicity, and Scale to Next-Gen IoT
For more than a decade, wireless microcontrollers (MCUs) have been evaluated primarily on radio performance. Range, sensitivity, protocol support, and transmit power defined leadership. These metrics still matter, but in modern IoT systems, connectivity is no longer the primary constraint. System complexity is.
Rethinking the Role of the IoT MCU
Today’s IoT products are expected to deliver more intelligence, tighter power efficiency, and faster time to market, all while reducing cost. Yet many designs still rely on multiple MCUs operating on the same board. A single device might have one MCU for connectivity, another for application control, and a third for real-time processing. And sometimes a fourth is required for sensing or device management.
This architecture persists because it’s familiar. But it’s far from optimal.
As IoT systems evolve, RF performance alone is no longer the defining metric. What matters today is how efficiently the entire system is architected.
Silicon Labs Series 2 was designed around the premise that wireless MCUs should not just connect devices, but consolidate them.
The Hidden Inefficiency in Today’s IoT Designs
A typical connected device often includes:
- A wireless SoC for Bluetooth Low Energy (LE), Zigbee, Thread, or proprietary connectivity
- An application MCU for control logic
- A motor-control MCU for deterministic actuation
- A low-power controller for sensing or housekeeping
Each additional device increases:
- Bill-of-material cost (BOM)
- PCB area
- Firmware complexity
- Validation effort
- Inter-processor latency
- Idle and leakage power
Ironically, much of this duplication is unnecessary. Wireless workloads are event-driven and burst-based. In many systems, the connectivity stack consumes a fraction of available CPU cycles. The processor becomes active during packet handling, then remains idle for extended intervals.
This creates a structural inefficiency. Significant compute headroom remains unused while additional MCUs are added elsewhere on the board. This presents an opportunity to reclaim that headroom and consolidate system functionality without compromising wireless performance.
Consolidation Only Works if Isolation is Guaranteed
The primary reason many systems remain partitioned is concern. Engineers hesitate to combine workloads for fear of degrading wireless determinism or introducing timing jitter into real-time tasks.
Silicon Labs Series 2 addresses this directly. It employs a multicore, event-driven architecture with functional separation:
- Dedicated cores manage radio and security operations
- Latency-critical wireless tasks execute independently
- The application core remains available for control, sensing, and AI workloads
This separation ensures that adding application functionality does not degrade wireless performance or real-time behavior. Instead of protecting RF integrity through partitioning, designers can now protect it through architecture.
Event-Driven Compute: Doing More with Less Power
Reducing component count is only part of the system equation. Power efficiency is equally critical. Traditional MCU-based systems rely heavily on CPU intervention. Interrupt-driven designs wake the processor frequently, increasing dynamic power consumption and adding software overhead.
Series 2 takes a fundamentally different approach.
Its Peripheral Reflex System enables peripherals to communicate directly with one another. Hardware events trigger hardware responses. Data can move through DMA pathways without waking the CPU.
For example:
- An ADC conversion can automatically initiate a memory transfer
- A comparator event can directly adjust a PWM output
- Timers can coordinate control loops autonomously
The processor wakes only when meaningful computation is required. This architecture delivers:
- Lower dynamic power consumption
- Deterministic real-time behavior
- Higher effective compute utilization
More work is done in hardware, so less energy is spent orchestrating it in software. In battery-powered and energy-sensitive systems, this is a structural advantage.
Real-Time Control and Connectivity on One Chip
Motor control illustrates the consolidation challenge clearly.
Closed-loop Field-Oriented Control (FoC) demands precise timing, high-speed ADC sampling, and coordinated PWM updates. Historically, this required a dedicated MCU to guarantee deterministic performance.
Series 2 challenges that assumption.
By combining advanced PWM peripherals, high-performance ADCs, hardware-based event routing, and efficient Arm Cortex-M33 processing, Series 2 can execute closed-loop FoC while simultaneously maintaining a Bluetooth LE stack on the same device.
This enables:
- Single-chip motor and wireless designs
- Reduced system latency
- Simplified firmware architecture
- Lower PCB complexity
For customers, the impact is direct:
- BOM reduction
- Lower power consumption
- Shorter validation cycles
- Faster time to market
The economics of intelligent devices shift when real-time control and connectivity coexist on one platform.
Embedded AI Without Additional Silicon
The next generation of IoT systems requires local intelligence. Sensor fusion, anomaly detection, predictive maintenance, and signal classification are increasingly moving from cloud to edge.
Traditional approaches add hardware. External NPUs or larger application processors increase cost, board space, and power complexity.
Series 2 integrates a Matrix Vector Processor (MVP) optimized for linear algebra, DSP workloads, and neural network inference.
By offloading math-intensive operations:
- CPU cycles remain available for control and connectivity
- Inference latency becomes predictable
- Energy per inference is significantly reduced
AI becomes a native system capability rather than an architectural add-on. Intelligence is integrated, not appended.
Platform Consistency That Scales
Architectural consistency is as important as performance.
Series 2 capabilities extend across Bluetooth, multiprotocol, sub-GHz, and proprietary families. Motor-control peripherals, AI acceleration, event routing, and security architecture are shared across the portfolio.
This enables:
- Software reuse across product variants
- Reduced SKU proliferation
- Simplified qualification processes
- Faster feature scaling
As organizations expand product lines or enter adjacent markets, a consistent platform reduces both technical and operational friction. Platform continuity becomes a multiplier for engineering productivity.
Connectivity is No Longer the Edge of the System, It’s at The Center
Many vendors approach connectivity by adding radios to traditional MCU architectures.
Series 2 takes the opposite path by absorbing application compute, control logic, and AI into the wireless platform itself. Instead of adding features through more silicon, the objective becomes removing silicon entirely.
In modern IoT systems, leadership will be measured by:
- How many components can be eliminated
- How efficiently compute headroom is utilized
- How intelligently power is managed
- How seamlessly functionality scales
A New Definition of the Wireless MCU
Series 2 redefines what a wireless MCU can be. A connectivity platform, an application processor, a real-time control engine, and an embedded AI accelerator. All within a single, power-efficient architecture optimized for real-world IoT systems.
As IoT architectures continue to consolidate, the question is no longer whether wireless MCUs should do more.
The real question becomes, how efficiently can they replace the rest of the system?
Series 2 was designed for this future from day one.
In modern IoT design, the most valuable innovation may not be what is added to the board, but what can finally be removed.