The Future of Motor Systems is Defined by Wireless Compute

A Consolidated Compute Platform for Modern Motor Systems

03/05/2026 | Jayant Jyoti | 3 Min Read

Motors power billions of devices across homes, industry, agriculture, and consumer products. For decades, motor architectures were optimized around one primary objective: control performance. Connectivity, analytics, and intelligence were layered on only when necessary.

That model is reaching its limits because today’s motor-driven products are expected to connect, adapt, update securely, and respond intelligently to changing conditions. They’re no longer isolated control nodes, but intelligent endpoints within broader digital systems. This evolution requires more than better control algorithms. It requires integrated wireless, compute, and machine learning (ML) at the core of the motion system.

Silicon Labs’ MG24-based connected motor solution represents this architectural shift.


Why Traditional Motor System Architectures No Longer Scale

Historically, connected motor systems were assembled from multiple components:

  • A dedicated motor-control MCU
  • A separate wireless SoC or module
  • Optional security elements
  • Additional processors for sensing or analytics

While functional, this fragmented model increases bill of materials (BOM) cost, PCB footprint, firmware complexity, and system latency. More importantly, it divides processing responsibility across devices, making feature expansion more difficult over time.

Adding wireless commissioning, over-the-air (OTA) updates, predictive diagnostics, or anomaly detection often requires redesigning system architecture rather than extending it. At the same time, product expectations have expanded. Modern motor-driven devices must be:

  • Wirelessly connected for configuration and diagnostics
  • Secure and field-updatable
  • Capable of local analysis and intelligent response
  • Compact and energy-efficient
  • Cost-optimized for scale

Meeting all these requirements with a multi-chip approach is increasingly inefficient.


MG24: A Wireless Compute Platform for Connected Motion

MG24 Multiprotocol Wireless SoC is designed for mid-range, connected motor systems where integration, efficiency, and intelligence drive differentiation.

MG24 consolidates the following all within a single SoC:

  • Real-time BLDC Field-Oriented Control (FOC)
  • Bluetooth Low Energy (LE) connectivity
  • Hardware-based security with Silicon Labs Secure Vault
  • DSP capability and machine learning acceleration
  • Event-driven hardware subsystems such as PRS and LESENSE

This integration enables a unified architecture where motion control, wireless communication, and intelligent processing operate together without competing for system resources.


Deterministic Motion Meets Wireless Responsiveness

Running real-time FOC alongside an active Bluetooth stack traditionally required separate processors to consistently meet tight control loop deadlines. The MG24 demonstrates that this separation is no longer necessary by maintaining precise motor control while sustaining wireless communication and application-level processing.

Designers can build connected motion systems without worrying that protocol activity will disrupt time-critical control loops. This balance is fundamental to next-generation wireless compute architectures for motion.


Intelligence at the Edge

As motion systems become connected, they must also become aware. With integrated DSP capability and the Matrix Vector Processor (MVP) hardware accelerator, MG24 enables local data processing for:

  • Vibration analysis
  • Anomaly detection
  • Predictive maintenance
  • Performance optimization

By processing data at the edge, systems can respond immediately to mechanical changes, reduce cloud bandwidth, and improve overall efficiency. Motor-driven products evolve from executing commands to making informed decisions.


Hardware-Level Event Handling for Efficiency and Stability

The Peripheral Reflex System (PRS) and LESENSE allow hardware-triggered responses to motor and sensor events without CPU intervention. This event-driven design reduces latency, improves stability, and optimizes power consumption. It also frees processing headroom for higher-level functionality, strengthening the overall system architecture.


Security as a System Foundation

Connected devices must be trusted over their lifetime. MG24 integrates Secure Vault™ with PSA Level 3 certification, ensuring secure boot, protected key storage, device identity, and encrypted OTA updates. This security foundation enables large-scale deployment of connected motor systems with confidence.


Demonstration: Wireless Compute Controlling Motion in Real Time

The architectural shift becomes clear in this demonstration.

In this showcase, a BLDC motor is controlled entirely by a single MG24 device. The SoC executes real-time FOC while maintaining active wireless communication.

During operation, external mechanical interference is introduced. The system detects the anomaly immediately and safely stops the motor. Once normal conditions return, it resumes operation automatically. A connected mobile device provides live interaction and visibility into system behavior throughout the process.

What traditionally required separate controllers for motor control, connectivity, and supervisory logic is consolidated into one integrated wireless compute platform. The demonstration highlights how architectural integration improves responsiveness, safety, and system simplicity simultaneously.


Enabling the Next Generation of Connected Motion

This approach unlocks new possibilities:

  • Smart shades that detect increased resistance and prevent wear
  • Fluid-handling pumps that identify cavitation and adjust proactively
  • Power tools that monitor vibration signatures for maintenance alerts
  • Actuators that receive firmware updates wirelessly to improve performance

In these applications, differentiation comes from integration and intelligence, not just torque precision.


Where This Architecture Delivers Immediate Value

The impact is strongest in mid-range, high-volume markets where size, efficiency, and connectivity are essential:

Smart Home and Building Automation

Curtains, blinds, vents, compact robotics

Light Industrial and IoT Automation

Actuators, valves, small conveyors

Connected Tools and Appliances

White goods, power tools

Smart Agriculture

Pumps, irrigation systems, feeders

In each category, consolidating motion, connectivity, and intelligent processing into a single device reduces complexity while expanding capability.


A Platform Approach to Motor Systems

The future of motor systems will not be defined solely by faster control loops. It will be defined by integrated platforms. By combining motion control, wireless connectivity, security, and edge intelligence within one architecture, manufacturers can:

  • Accelerate development cycles
  • Simplify hardware design
  • Enable fleet-wide OTA updates
  • Introduce predictive maintenance and service-based business models

MG24 represents this evolution toward wireless compute-driven motion systems.


One Device. Unified Architecture. Scalable Innovation.

Every motor that benefits from connectivity will ultimately require more than a standalone controller. MG24 demonstrates how a single secure, wireless-enabled platform can replace fragmented multi-chip designs and enable smarter, more adaptable products. As connected systems continue to evolve, wireless compute will sit at the center of motion, enabling a new generation of intelligent, integrated devices.

Jayant Jyoti
Jayant Jyoti
Senior Product Marketing Manager
Close
Loading Results
Close