Wi-Fi Developer Journey

Developing with Low Power Wi-Fi

The low power features available in the latest Wi-Fi standards mean that a lot of today’s IoT devices are "always-on" and connected, with extended battery life due to ultra-low power consumption. Wi-Fi 6 standard introduced several features that are the enablers for devices to go into low power states, stay dormant longer and transfer data more efficiently than earlier Wi-Fi generations.

Operational Modes

Wi-Fi SoC, RCP, and NCP modes refer to different operational modes for Wi-Fi, each with its own specific use cases and configurations:

SoC - MCU For Application

  • Application, Wireless, and networking stacks run on SiWG917
  • No external host needed​
  • Optional: Dual Stack. Maintain TLS/TCP connection for an external host
SoC (System on Chip) Mode

Network Co-Processor

  • Hosted – Network Co-Processor (NCP)
  • ​Host MCU runs RTOS, application code, cloud agent, and Matter
  • ​SiWN917 runs Wi-Fi and Bluetooth radios, wireless and networking stacks
Network Co-Processor (NCP) Mode

Radio Co-Processor

  • Hosted - Radio Co-Processor (RCP)
  • SiWT917 radio transceiver mode for Wi-Fi and Bluetooth
  • ​Linux host runs wireless, networking, and security stacks​
Radio Co-Processor (RCP) Mode

Wi-Fi Developer Journey with Silicon Labs

Silicon Labs can accelerate the development of Wi-Fi devices, starting by outlining each step in the process and helping you along each stage of your project. We are here to simplify your development journey and help you get your devices to market faster and more efficiently.
We have outlined below three key stages of the Wi-Fi Developer Journey, along with what is required to successfully complete each stage.

Getting Started
Develop
Deploy Product
  1. 1. Buy Kit: Hardware
  2. 2. Download Development Tools
  3. 3. Out of the Box Demo
  1. 1. Create a Sample Application
  2. 2. Develop and Debug
  3. 3. Test and Iterate
  1. 1. Qualify Product (Certification)

1. Buy Kit: Hardware

Silicon Labs offers several Wi-Fi development kits ranging from a low-cost small form factor prototyping platform to a feature-packed development platform kit for advanced application development. There's also development platforms options for Network Co-Processor (NCP) modes of operation. Select one kit that best fit your needs.

 
KitSiWx917 Wi-Fi 6 and Bluetooth LE 8 MB Flash SoC Pro Kit
SiWx917 Wi-Fi 6 and Bluetooth LE 4MB Flash Co-Processor Radio BoardSiWx917 Wi-Fi 6 and Bluetooth LE Dev KitSiWx917Y Module Wi-Fi 6 and Bluetooth LE Explorer Kit
OPN(SiWx917-PK6031A)(SiWx917-RB4346A)
+
Si-EB8045A, Si-EB8045B, Si-EB8045C
(SiWx917-DK2605A)(SiWx917-EK2708A)
Target DeviceSiWG917M111MGTBASiWN917M100LGTBASiWG917M111MGTBASiWG917Y111MGA
On-chip Memory8 MB Flash4 MB Flash8 MB Flash8 MB Flash and 8 MB PSRAM on board
RF Front-endExternal SwitchExternal SwitchExternal SwitchIntegrated Switch
RF Test ConnectorYesYesYesNo
Energy Monitor (AEM)Yes—OptionalOptional pads for 10-pin connector
Operational ModeSoC ModeNCPSoC ModeSoC Mode
Packet Traffic Arbitration (PTA)—Yes——
On-board DebuggerAdvanced—BasicBasic
Debug In/OutYes/YesYes/NoYes/NoYes/No
User Buttons & LEDsYes—YesYes
Breakout Pads
(Pins Accessible)
Yes (Full Pin Access)Yes (Limited Pin Access)Yes (Limited Pin Access)Yes (Limited Pin Access)
DisplayYes———
On-board SensorsYes—YesNo
3rd Party Hardware Addons——YesYes

Note: Silicon Labs offers other Wi-Fi products, view them all here.

< Previous Step Next Step >

2. Download Development Tools

Set up your development environment with Silicon Labs development tools.

Simplicity Connect Mobile App

Test and debug Wi-Fi embedded applications quickly - including OTA updates, data throughput, and Android and iOS interoperability. Download Simplicity Connect app on your smartphone and speed up development now. 

Android/Google Play Store

iOS/Apple App Store

efr-app-demo.jpg
< Previous Step Next Step >

3. Out of the Box Demo

The out-of-box demo is pre-flashed on your SiWx917 radio board. This guide describes how to get started with running the out-of-box demo for the SiWx91x chipset family using the WiSeConnect SDK in System-on-chip (SoC) mode, where both the application and the connectivity stack run on the SiWx91x chipset.

Out of the Box Demo - SiWG917 (GitHub)

This application demonstrates the WLAN, BLE, MCU peripheral features and NWP (network processor) powersave capabilities of SiWG917 Pro Kit with a ready to go, minimal software installation experience.

Suggested Kit:

Additional Resources:

< Previous Step Next Step >

1. Create a Sample Application

Developing a Wi-Fi IoT application begins with creating a sample application. Here is a collection of instructions and guides to help you start coding your sample application.

The WiSeConnect SDK getting started page guides you through the first steps of application development in all the operational modes: System-on-chip (SoC), Network Co-Processor (NCP), and Radio Co-Processor (RCP). It also covers the first steps of Matter software development.  

Should you want to study our Wi-Fi software architecture, you can start by reading our Software Reference guide.


For information about the security, you can refer to the below documents:

Here are some additional documents that you might find helpful in application development:

< Previous Step Next Step >

2. Develop and Debug

When you are ready to begin your Wi-Fi IoT application development and debugging, these resources will be helpful during your project.

Here is a collection of the basic software development instructions and guides:

For hardware design considerations such as choosing the right crystal, please check the following documents:

For antenna design and optimization consideration, please refer to the below documents:

For hardware debugging, you might find the following documents helpful:

< Previous Step Next Step >

3. Test and Iterate

It is important to test your Wi-Fi IoT application code before submitting it to test labs to ensure it will pass testing. These resources will help you to achieve test compliance.

Our manufacturing utility guide covers various device configuration aspects such as memory, security, flashing, and much more:

How to run throughput tests in NCP mode? Please check our AN1434: SiWx917 NCP Throughput to find out.

For final RF adjustments, please check our AN1440: SiWx917 Gain Offset Calibration guide.

Outlines the manufacturing procedure for the SiWx917 NCP IC (SiWN917M) / Module (SiWN917Y) using Silicon Labs' manufacturing utility.

< Previous Step Next Step >

1. Qualify Product (Certification)

 

< Previous Step Next Step >
Getting Started
1. Buy Kit: Hardware
2. Download Development Tools
3. Out of the Box Demo
Develop
1. Create a Sample Application
2. Develop and Debug
3. Test and Iterate
Deploy Product
1. Qualify Product (Certification)
Close
Loading Results
Close